Skip to main content
Associate II
Apr 30, 2026 10:01 AM UTC
Question

STM32CubeMonitor-Power: Add Logarithmic Scaling ?

I have a suggestion for the STM32CubeMonitor-Power application.

For the ultra low power applications it would be great if the Y-axis could be logarithmically scaled, so that the area around 0.5-100 µA is more detailed (sleep mode) compared to the active mode (1-2 mA). As it is now I cannot quantify the current usage with a glance when the device is sleeping.

I would very much like this to be added.

Greetings,

Rico