Skip to main content
acv_atr
Associate III
Mar 23, 2022 11:33 AM UTC
Solved

STM32CubeMonitor 1.4.0 CPU critical performance issue

Hello everyone.

I'm trying to work with STM32CubeMonitor to implement an industrial machine Life Test JIG using 12 ST-LINK v2 probes connected to STM32 microcontrollers by SWD protocol, but I'm facing very strange and anoying issues.

This post will focus only on CPU critical allocation on V1.4.0.

When acq node is started (only after receive start acquisition order) the process allocate 100% of one CPU core.

As shown on the picture below, I'm using at the moment and for development purposes, only two ST-LINK probes, that's why "only" two cores are at 100% allocation.

0693W00000Kdj6MQAR.png 

This does not occurs on STM32CubeMonitor V1.3.0

0693W00000Kdj75QAB.png 

According to V1.4.0 release notes the multiple probe acquisitions was improved.

0693W00000Kdj8NQAR.png 

Windows 10 pro has the same behaviour on V1.3.0 and V1.4.0

Ubuntu 20.04 Desktop has also been tested and verified.

All installation recomendations defined at wiki have been meet.

Question: Is this CPU allocation expected/known and it's a true improvment relative to v1.3.0?

This topic has been closed for replies.
stephane.legargeant
ST Employee
Oct 31, 2022 5:06 PM UTC

Hello

Problem should be fixed in version 1.5.0: For frequency lower than 10Hz, the thread will give back the free time to the CPU, and the CPU usage will decrease.

Please let us know if it is good for you.

Best regards

Stephane

14 replies

acv_atr
acv_atrAuthor
Associate III
May 17, 2022 7:50 PM UTC

Hello @Richard.Chvr​ .

Any news from dev team or next stm32cubemonitor release?

Thank you for your support and attention.

acv_atr
acv_atrAuthor
Associate III
Jun 27, 2022 10:38 AM UTC

Hi Mr. @Richard.Chvr​ 

Have you already avalilble some news or solutions from dev team?

Thanks for your attention.

Best regards

Richard.Chvr
ST Technical Moderator
Sep 22, 2022 8:07 AM UTC

Hi,

In next release 1.5.0, it will will possible to get 2 different modes, either to optimize acquisition frequency or CPU workload depending on a user setting.

Coming soon...

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
stephane.legargeant
ST Employee
Oct 31, 2022 5:06 PM UTC

Hello

Problem should be fixed in version 1.5.0: For frequency lower than 10Hz, the thread will give back the free time to the CPU, and the CPU usage will decrease.

Please let us know if it is good for you.

Best regards

Stephane