Skip to main content
grisom13
Associate III
November 11, 2025
Solved

STM32Cube Monitor USB PD

Hello,

I am trying to use STM32Cube Monitor USB PD with custom board.

I see ST link v3 minie on a trace port. but I can't see any traces at all. Is there a dedicated package in CubeMX i can enable to see USB-PD traces ? Thank you. 

Screenshot 2025-11-11 at 11.03.56.png

PPAIL.1
PPAIL.1Best answer
ST Employee
November 14, 2025

Hi @grisom13

 

I confirm USART1 should work with STM32CubeMonitor UCPD.

For further help please share your ioc.

-------------------

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

 

 

5 replies

grisom13
grisom13Author
Associate III
November 11, 2025

Ok, looks like the Trace enable in under Utilities section 

 

 

UPD. Added code by Cube MX. I see the USART1 rate changed to 921600 from 115200 in Main.C but still the Trace screen is empty.

 

I am following the below article:
https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB-Power_Delivery_Source

1 - I am using USART1 115200, not LPUART  - is this OK ?

2- Do i need to unable GUI for USBPD monitor ? 

 

 

grisom13
grisom13Author
Associate III
November 13, 2025

No Advise ? :(

PPAIL.1
ST Employee
November 13, 2025
Hi @grisom13
 
On a Nucleo-G071RB board, using USART1 instead of LPUART1 could be the cause of the problem as USART1 do not use the same pins than LPUART, so is not connected to ST link.
 
However, you are using a custom board, which MCU are you using ?
Please could you share your .ioc, and schematic ?
 
 
grisom13
grisom13Author
Associate III
November 13, 2025

Hello,

I have STM32G0B1KBU3N MCU. Currently my Custom PCB has only USART1. RX and TX pins connected to ST Link V3 minie. Please confirm this can work with USB-PD STM32 monitor. 

PPAIL.1
PPAIL.1Best answer
ST Employee
November 14, 2025

Hi @grisom13

 

I confirm USART1 should work with STM32CubeMonitor UCPD.

For further help please share your ioc.

-------------------

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.