Skip to main content
Inigo
Associate II
May 22, 2021 7:52 AM UTC
Solved

STM32Cube Monitor: Serial Out

Hello,

I'm new to STM32CubeMonitor and I need some help.

I made a project that consists of sending an unkown length string (DMA) to a nucleo board and then receive the same message on my terminal.

I've been using realterm and it works fine, but i would like to know how to send strings using STM32CubeMonitor software.

I want to type a message on a 'text input' node, press a button and then send the string to the board.

Thank you,

Iñigo

This topic has been closed for replies.
Richard.Chvr
Richard.ChvrBest answer
ST Technical Moderator
Sep 27, 2023 1:51 PM UTC

No update since a while, closing the post.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

3 replies

LMI2
Senior III
May 22, 2021 12:03 PM UTC

I wonder if CubeIDE has a serial monitor. It should have.

Inigo
InigoAuthor
Associate II
May 22, 2021 3:26 PM UTC

It is possible to install a terminal in CubeIDE, but i want to send strings to the board using CubeMonitor. I'm designing a robot arm which will be used by university students (i'm a student too). They must be able to visualize variables and send commands to control the robot (they dont need CubeIde). It will be great if they can do both things using only CubeMonitor.

Richard.Chvr
Richard.ChvrBest answer
ST Technical Moderator
Sep 27, 2023 1:51 PM UTC

No update since a while, closing the post.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.