Skip to main content
This topic has been closed for replies.
Richard.Chvr
Richard.ChvrBest answer
ST Technical Moderator
Sep 27, 2023 1:43 PM UTC

No update since a while, closing the post.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

3 replies

stephane.legargeant
ST Employee
Oct 8, 2020 7:35 AM UTC

Hello

It seems that node-RED need to have a "default" section after the users. Else the design windows may not be displayed. Have you defined one ?

adminAuth: {
 type: "credentials",
 users: [ /*your list of users */ ],
 default: {
 permissions: "read"
 }
}

Can you try ?

Best regards

Stephane

victagayun
Senior III
Oct 8, 2020 10:45 PM UTC

Thanks for the reply.

Actually, I do not want them to view my flows too.

Yes, I tried that. It is still possible to view / read only the flows.

I was trying to change the root path of the UI from

http://localhost:1880/ui

to, say something like:

http://localhost:1880/dontview

by un-commenting

httpAdminRoot: '/dontview',

I was able to view the new "url" and save the flows but the dashboard wont display the data.

BTW, the Cubemonitor will not show up and display "Error" on it title bar but using the browser, I was able to edit and save the flow.

Only the problem is when I click the dash board, data wont show up especially the line graph.

Gauge seems to display, but I cannot confirm if data is correct as I was concentrating on the line graph.

Richard.Chvr
Richard.ChvrBest answer
ST Technical Moderator
Sep 27, 2023 1:43 PM UTC

No update since a while, closing the post.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.