Skip to main content
Visitor II
Feb 26, 2024 10:11 AM UTC
Question

Give an example to change the value of a variable in the target thread

To test control the device, I need to change the values of some variables using dashboard elements.

"Write Panel" doesn't work for me.
Show me an example of how to implement it? Thank you!

AlexArGC_0-1708941768893.png

"Write Panel" tried to generate a payload of the format:

 

{
 "variablelist": [
 {
 "address": "0x20003954",
 "name": "alg::apiControls.valves.registr",
 "type": 1,
 "checked": true,
 "$$hashKey": "object:153",
 "value": "1",
 "validity": true
 }
 ],
 "accesspoint": 0
}

 

What is "$$hashKey": "object:153" ?

This value is always new, after each deployment.

 

 

 
    This topic has been closed for replies.

    1 reply

    stephane.legargeant
    ST Employee
    Feb 27, 2024 8:54 AM UTC

    Hello

    The $$hashKey is added by angular framework and it is not used by the probe out node. You can ignore it.

    The value seems ok for a unsigned int8 at address 0x20003954, and it should be set to 1.

    There is a red triangle on the MyVariables node, can you check it ?