Skip to main content
MKori.1
Associate III
Aug 14, 2023 3:09 PM UTC
Solved

Get exefile parameter from "variables"-node

Hello,

I'm using the current version of STM32CubeMonitor (1.6.0) under Windows and would like to check in my flow if the configured exefile in the STMicroelectronics variable node is the intended one (e.g fits a regex). For this I would like to read out the exefile parameter. Using a debug-node I can see it is written but 'undefined'.
Is there a workaround for this or is it possible to give the exefile as input parameter to the variable node?
My output looks like this: 

 

object
groupname: "STM32G0 Binary Production"
variablelist: array[19]
mode: "direct"
snapshotheader: ""
triggerstartmode: "manual"
triggername: "my_unused_variable"
triggerthreshold: ""
frequency: 10
accesspoint: 0
exefile: undefined

 

Thank you!

    This topic has been closed for replies.
    Richard.Chvr
    Richard.ChvrBest answer
    ST Technical Moderator
    Sep 7, 2023 9:32 AM UTC

    Hello @MKori.1 

    The fact that exefile appears as undefined is a known bug that will be fixed in next 1.7.0 release planned in a short term.

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    3 replies

    Richard.Chvr
    ST Technical Moderator
    Aug 31, 2023 2:45 PM UTC

    Hello @MKori.1,

    I'm afraid, it's not possible to give exe file as input parameter of the variable node. May be you can try a solution using regexp-filter in order to verify your file.

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    MKori.1
    MKori.1Author
    Associate III
    Aug 31, 2023 3:01 PM UTC

    Hello @Richard.Chvr ,

    thank you for your response. Yes, this together with a .json parser this is my current solution. It has some drawbacks, for instance when mulitple exefile configurations are defined checking the correct one is some additional effort.
    What is about the empthy "exefile" output of the node? Is there some information output planned?

    Richard.Chvr
    Richard.ChvrBest answer
    ST Technical Moderator
    Sep 7, 2023 9:32 AM UTC

    Hello @MKori.1 

    The fact that exefile appears as undefined is a known bug that will be fixed in next 1.7.0 release planned in a short term.

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.