Skip to main content
Senior III
September 20, 2025
Question

Difficulty to watch the variables disabled in cubemonitor

Iam using cube monitor which is off course a very useful tool for debugging but only difficulty iam facing is when i disable the variables which i don't want to see or completely invisible, could you please bring in something so that it can be visible even if disabled. Ex image below

STuser2_0-1758363255074.png

If you see above image the disabled variables are completely invisible for me to make them enable again.

 

    This topic has been closed for replies.

    2 replies

    Richard.Chvr
    ST Technical Moderator
    September 25, 2025

    Hello @STuser2 

    You would like to have an option to hide/unhide variables from the graph upon clicking on their name, is that right?

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    STuser2Author
    Senior III
    September 25, 2025

    What i am trying to say is that even if i make variables as hidden, after some time i may want to watch the variables (hidden) again so it should be partially visible instead of completely hidden.