Skip to main content
BPere.1
Associate
Apr 8, 2023 2:39 PM UTC
Question

Can a variable be modified by using it's name instead of it's address?

Hard coding address for variables could be problematic as the linker can move them during development. Is there a way to write a variable using its name instead of its address? The variables node has this information. How can I use the name in a templet to change the value of a variable?

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
Apr 8, 2023 3:52 PM UTC

Should be in object file as a symbol.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
S.Ma
Principal
Apr 8, 2023 6:39 PM UTC

Mayve start from what do you want to achieve rather than one method which might not be the best solution. Magling through object, map or elf file seems weird.

Georgy Moshkin
Senior
Aug 24, 2023 9:09 AM UTC

Yes, it is possible by using little helper function node. You can try my WriteByName v1.0 node (tested in STM32CubeMonitor 1.6.0).

https://youtu.be/B6R8yJ6DEQo

Download node source code (can be imported in cube monitor): nodes10.zip - nodes for STM32CubeMonitor 

How it works: on the first run all variable names are used to build global variables with JSON messages. Those JSON messages contain variable memory address and type. When buttont/text is entered, this JSON message "value" is modified and sent to "acq out" / "probe out".

 

Check my STM32 Bootloader - flash your STM32 with AES-encrypted binaries right from web browser!