Skip to main content
chriskuku
Senior II
Apr 12, 2025 8:59 AM UTC
Question

Yellow flagged pin conflict information pops up too short to read (macOS)

When being in the MX (.ioc) file view hovering over a yellow marked TIM1 e.g., a grey field pops up for half of a second. I'm hardly able to read and understand the sense, too short is the presence of that field. Can it be looked up elsewhere in the GUI. It says something of "partly disabled,a conflict with PB13 being used as an output" or so.

 

This topic has been closed for replies.

3 replies

TDK
Apr 12, 2025 12:56 PM UTC

PB13 can be TIM1_CH1N. If you're using the pin as GPIO, this channel of the timer can't be enabled.

The yellow flags do not indicate errors, just that you can't do something because a pin is being used. They can be safely ignored as they do not indicate an error.

"If you feel a post has answered your question, please click ""Accept as Solution""."
chriskuku
chriskukuAuthor
Senior II
Apr 29, 2025 7:30 AM UTC

Thanks. My question was: why does the tooltip flash up too shortly to read it. Is it a macOS problem/issue?

 

TDK
Apr 29, 2025 1:38 PM UTC

Yes, it seems to be a MacOS-specific issue.

"If you feel a post has answered your question, please click ""Accept as Solution""."