Skip to main content
lenonrt
Associate III
November 3, 2019
Question

X CUBE AWS STM32 Discovery kit - IoT node

Hello,

I'm trying to compile the firmware to use the B-L475E-IOT01A in AWS IoT.

I just download the pack X CUBE AWS, import to STM32CubeIDE(v1.0.0 and v1.1.0) and compile.

There are two error on make file.

I try to make the samething with SW4STM32(v2.9 and v2.8), and the same problem appears.

make[1]: *** [makefile:88: post-build] Error 1
make: *** [makefile:55: all] Error 2

Obs.: I need to atualize the firmware because I have an old version and don't work on AWS IoT.

This topic has been closed for replies.

2 replies

Guillaume K
ST Employee
November 22, 2019

Which version of X-CUBE-AWS are you using ? 1.4.0 ?

From the log the post-build script failed.

The postbuild is used to create a big binary file with SBSFU boot loader and the application concatenated together.

Normally the SBSFU post-build script creates an "output.txt" file in directory SW4STM32. What is the content of this file ? It can give some hint about the problem.

did you install STM32 Cube Programmer v2.x ? it is required to create the SBSFU+application binary.

Also are you on Windows or Linux ? On Windows the postbuild script is a python script pre-compiled in an .exe file. It should run alone.

On Linux the python script is used directly so you need python to run it.

lenonrt
lenonrtAuthor
Associate III
December 12, 2019

Hi @Guillaume K​ !

I'm using Windows. I have STM32 Cube Programmer installed.

I found on X CUBE AWS folder a compiled filed, so I just use that.

Thank you!

Lenon