Skip to main content
LMI2
Senior III
May 25, 2021 6:40 PM UTC
Solved

Wrong version number of CubeIde shown

I have CubeIde 1.61 installed on Win10/64 hard disk. About box/dialog says it is version 1.61, that is, the current version. Desktop icon or shortcut says it is version 1.40 or something. That is the original version number I installed sometime ago and then later updated.

I can change the name easily, so that is not the problem. Perhaps the shortcut should only be named CubeIde?

This topic has been closed for replies.
Pavel A.
Pavel A.Best answer
May 25, 2021 7:24 PM UTC

This is a known issue. TL;DR not a bug, won't be fixed.

Instead, to know what is the true version (besides the About dialog), open the file stm32cubeide.ini in the CubeIDE dir.

Look for line like:

-Declipse.buildId=Version 1.6.0

This gives the actual version.

--pa

4 replies

Pavel A.
Pavel A.Best answer
May 25, 2021 7:24 PM UTC

This is a known issue. TL;DR not a bug, won't be fixed.

Instead, to know what is the true version (besides the About dialog), open the file stm32cubeide.ini in the CubeIDE dir.

Look for line like:

-Declipse.buildId=Version 1.6.0

This gives the actual version.

--pa

LMI2
LMI2Author
Senior III
May 26, 2021 5:21 PM UTC

MS style: a feature, not a bug.

Piranha
Principal III
Jun 5, 2021 1:29 PM UTC

Polluting the user's Desktop and other private folders with shortcuts is actually a leftover from 90s, when it was "cool" to pollute everything with a zillion toolbars, pop-ups, shortcuts and whatnot.

https://github.com/postmanlabs/postman-app-support/issues/6604

Cartu38 OpenDev
Graduate II
Jun 5, 2021 7:46 PM UTC

@Piranha​ unfair & useless comment ...

STM32CubeIDE installer is asking you if you want or not shortcut setup ....