Skip to main content
Nikita91
Lead II
May 24, 2020
Question

Will ST review the HAL and LL files to remove all the warnings in it?

To compile I use the following flags:

-mthumb -mcpu=cortex-m4 -mfloat-abi=hard -mfpu=fpv4-sp-d16 -std=gnu99 -DSTM32F429xx -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_FULL_ASSERT -DHSE_VALUE=8000000 -DUSE_HAL_DRIVER -I../Application -I../AA -I../BSP/STM32F4 -I../aaBasic -I../tests -I../aaUtils -I../aaTests -I../system/include -I../system/include/device -I../system/include/cmsis -I../system/include/stm32f4-hal -I../lwip/src/include -I../lwip/system -Og -ffunction-sections -fdata-sections -g -fstack-usage -Wall -Wformat=2 -Wshadow -Wunused -Wlogical-op -Wconversion -Wsign-conversion -Wextra -pedantic -Wswitch-default -specs=nano.specs

The log window displays a lot of warning messages from HAL and LL files. All these yellow lines bother me and each time I have to go and see if one or 2 is not from my files. Some examples:

..\system\src\stm32f4-hal\stm32f4xx_ll_fmpi2c.c:221:0: warning: ISO C forbids an empty translation unit [-Wpedantic]
 
 
..\system\src\stm32l4p-hal\stm32l4xx_hal_rcc.c: In function 'HAL_RCC_OscConfig':
..\system\src\stm32l4p-hal\stm32l4xx_hal_rcc.c:946:1: warning: embedding a directive within macro arguments is not portable
 #if defined(RCC_PLLP_SUPPORT)
 ^
..\system\src\stm32l4p-hal\stm32l4xx_hal_rcc.c:948:1: warning: embedding a directive within macro arguments is not portable
 #endif
 ^
 
 
../system/include/stm32l4p-hal/stm32l4xx_hal_dma.h:85:42: warning: comma at end of enumerator list [-Wpedantic]
 HAL_DMA_STATE_TIMEOUT = 0x03U, /*!< DMA timeout state */
 ^
 
 
..\system\src\stm32f4-hal\stm32f4xx_ll_rcc.c: In function 'LL_RCC_GetRNGClockFreq':
..\system\src\stm32f4-hal\stm32f4xx_ll_rcc.c:752:42: warning: unused parameter 'RNGxSource' [-Wunused-parameter]
 uint32_t LL_RCC_GetRNGClockFreq(uint32_t RNGxSource)
 ^~~~~~~~~~
..\system\src\stm32f4-hal\stm32f4xx_ll_rcc.c: In function 'LL_RCC_GetUSBClockFreq':
..\system\src\stm32f4-hal\stm32f4xx_ll_rcc.c:847:42: warning: unused parameter 'USBxSource' [-Wunused-parameter]
 uint32_t LL_RCC_GetUSBClockFreq(uint32_t USBxSource)
 
..\system\src\stm32f4-hal\stm32f4xx_ll_adc.c:290:53: warning: unused parameter 'ADCxy_COMMON' [-Wunused-parameter]
 
 
..\system\src\stm32f1-hal\stm32f1xx_hal_tim_ex.c:1734:60: warning: unused parameter 'htim' [-Wunused-parameter]
 1734 | HAL_StatusTypeDef HAL_TIMEx_RemapConfig(TIM_HandleTypeDef *htim, uint32_t Remap)
 
../system/include/stm32f4-hal/stm32f4xx_ll_rtc.h:673:114: warning: conversion to 'unsigned int' from 'int' may change the sign of the result [-Wsign-conversion]
 673 | #define __LL_RTC_CONVERT_BCD2BIN(__VALUE__) (uint8_t)(((uint8_t)((__VALUE__) & (uint8_t)0xF0U) >> (uint8_t)0x4U) * 10U + ((__VALUE__) & (uint8_t)0x0FU))

It would be nice if HAL and LL compile properly ...

This topic has been closed for replies.

3 replies

TDK
May 24, 2020

Seems like sometimes they used UNUSED(...) to prevent unused parameter warnings, but not everywhere. I can't imagine it's a high priority.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Nikita91
Nikita91Author
Lead II
May 31, 2020

That's not much, but it shows that the quality process for software development at ST is not very rigorous.

And this little rigor is transmitted to our developments in these traces, which must be explained during each quality review ... The listeners' opinion: "You use ST software... Maybe you should do without it."

The perceptible quality of ST software would be better if there were no warnigs during compilation.

I notice that there is no response from ST when we talk about the quality of its software ...

Pavel A.
May 31, 2020

Precisely for this situation all decent lint tools have notion of "system libraries" - that's, external source outside of your control.

Apply this and cut the noise.

The decision whether to use the ST software, or roll your own, is up to you.

-- pa