Skip to main content
MPony.1
Associate
August 6, 2020
Question

Why this pity code at line 13 couse the Hard Fault?

#include "stm32f0xx.h"
void SysInit(void);
 
uint8_t array1[260] = {0};
uint8_t array2[260] = {0};
uint16_t test;
int main(void) {
	SysInit();
	for(uint16_t i = 0; i < 260; i++)
		array1[i] = i & 0xFF;
	test = *(uint16_t*)&array1[0xEA];
	test = *(uint16_t*)&array1[0xEC];
	test = *(uint16_t*)&array1[0xEB];
	while(1);
}
void SysInit(void) {
	FLASH->ACR |= FLASH_ACR_PRFTBE | FLASH_ACR_LATENCY;
	RCC->CR2 |= RCC_CR2_HSI48ON;
	while(!(RCC->CR2 & RCC_CR2_HSI48RDY)) {};
	RCC->CFGR &= ~(RCC_CFGR_PPRE | RCC_CFGR_HPRE | RCC_CFGR_SW);
	RCC->CFGR |= RCC_CFGR_PPRE_DIV16 | RCC_CFGR_HPRE_DIV1 | RCC_CFGR_SW_HSI48;
	while((RCC->CFGR & RCC_CFGR_SWS) != RCC_CFGR_SWS_HSI48) {};
	RCC->CFGR &= ~RCC_CFGR_PPRE;
	RCC->CFGR |= RCC_CFGR_PPRE_DIV1;
	SystemCoreClockUpdate();
}

Every other valid reading from the filed array1 works normaly (Except Index 0xEB). I tried almost everthing. (volatile, optimizer, additional variables, memory aglin etc.) This code works propely on other arm devices. I need this code for further purpose (writing to TX-SPI 16bit register).

MCU: STM32F072CBT

IDE: STM32CubeIDE, Keil

This topic has been closed for replies.

8 replies

mckenney
Associate
August 6, 2020

"&array1[0xEB]" (in context) generates an odd address, so a 16-bit access is unaligned.

Per DUI0497A Sec 3.3.4: "There is no support for unaligned accesses on the Cortex-M0 processor. Any attempt to perform an unaligned memory access operation results in a HardFault exception."

I'm not sure there are any ARM devices where unaligned accesses do what you want. (The ARM7/9 were especially weird.)

What do you want to accomplish here?

Uwe Bonnes
Chief
August 6, 2020

Isn't M3/4/7 supposed to allow unaligne access?

Tesla DeLorean
Guru
August 6, 2020

He's using a CM0(+) device, which doesn't tolerate this.

All CMx devices will fault on misaligned STRD/LDRD

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MPony.1
MPony.1Author
Associate
August 6, 2020

I need this code for SPI transfer. The only way how to trasmitt data in 16bit mode is by writing the data directly into SPI->DR as 16 bit word. Writting data as 8bit works propely, but for my application is it too slow. The array must be aligned as 8 bit because data is read from 8 bit SRAM. Is there a way how to align the 8bit array for correct 16bit mode? ((I will try to retype the array1 to 16bit and write data from SRAM as 8bit.))

Tesla DeLorean
Guru
August 6, 2020

Problem is you're reading ODD addresses, doesn't matter how 8-bit array is aligned if you're casting both ODD and EVEN elements to 16-bit

Typically with byte aligned/packed structures (say serial packet data or files) you memcpy() to an auto/local array with known alignment, typically 32/64-bit depending on how tightly it is held to ABI expectations.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
S.Ma
Principal
August 6, 2020

I would use something like this:

typedef union
{
 struct
 {
 uint8_t u8_buf[256];
 uint16_t u16_buf[128];
 } b; /*!< Structure used for bit access */
} myBuf_t;
 
__ALIGN_BEGIN
myBuf_t myAlignedBuffer;
__ALIGN_END

This is IAR (stable and code unaffected by SW tools "upgrade".

The buffer is memory aligned and can be accessed as 8 bit or 16 bit.

Does it help?

Piranha
Principal III
August 7, 2020

Actually you have two separate arrays there. Remove the struct and leave those arrays inside the union.

Anyway the cast to properly aligned addresses technically does the same.

Pavel A.
August 6, 2020

Does GCC compiler for ARM have some attribute to extract data via unaligned pointer?

Something like uint16_t v = *(uint16_t * __unaligned p)