Skip to main content
GMano.1
Associate III
December 8, 2023
Question

Why Flash to the target after press RESET button then code will run?

Hai:

I am using STMcube IDE 1.13.2 and TouchGFX 4.22.1 in my project. Once flash the program to the traget, If i given play but program not run. Once i press the RESET button or Power ON and OFF then it will work.

This happend only in 1.13.2 IDE version. 

What i do for this issuse? Kindly help me for this issuse.

 

Thanks & Regards

Govind M 

    This topic has been closed for replies.

    1 reply

    TDK
    December 8, 2023

    Debug it, see where execution is at. The cpu is likely doing something.

    You can attach the debugger without flashing/resetting if you modify the debug configuration.

    "If you feel a post has answered your question, please click ""Accept as Solution""."