Skip to main content
Antypas.Peter
Senior
Aug 30, 2023 12:08 AM UTC
Question

Why does STM32CubeIDE use Chromium and peg my CPU so high on MacOS?

I'm running IDE version 1.13.1 on MacOS 11.7.1 on a MBP with a dual core 2.8Ghz i7. Unlike every other IDE / CAD package that I use, STM32CubeIDE pegs my CPU really high and spins up the fans even when doing NOTHING. As in, there is no project open, no editors, no HW configuration, literally NOTHING.

Why?

 

Screen Shot 2023-08-29 at 5.05.10 PM.png

    This topic has been closed for replies.

    14 replies

    Visitor II
    May 7, 2025 2:58 PM UTC

    I've been noticing this a lot too, The mysterious 8 Chromium instances are (a lot of the time anyways) using more CPU than CubeIDE is!

    Darren Legge
    Associate
    Jun 30, 2025 2:06 PM UTC

    The same approach works on macos (presumably linux would be similar). Close STM32CubeIDE and...

    cd ~/.stm32cubeide/.jxbrowser-7.41.4/
    rm -rf *
    cd ..
    chmod 555 .jxbrowser-7.41.4/

    Restart the IDE and enjoy the silence.

    If you need anything that jxbrowser does in future then just reset the write permission (chmod 777) on the .jxbbrowser... folder and STM32CubeIDE will put the files back.

    CTapp.1
    Senior III
    Jul 24, 2025 9:44 AM UTC

    I've just noticed the same thing happens (another 8 Chromium threads) with CubeMX under Windows (and likely MacOS).

    However, that one is not quite so easy to solve as the corresponding .stm32cubeMX folder contains other stuff, but just removing write access to the .jxbrowser folder it contains (like the MacOS fix for the IDE) does the job.

    All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)