Skip to main content
m4l490n
Associate III
January 31, 2020
Solved

Why can't I install Segger JLink Utilities?

There is a big issue I'm facing. I just installed STM32CubeIDE 1.2.0 but then I get an error when trying to install JLink_Linux_V662_x86_64.deb

0690X00000Bx9WXQAZ.png

I absolutely need those tools because I also do development for other boards with Segger JLink probes.

What is going on? My system is Linux Pop!_OS 18.04 LTS x86_64

This topic has been closed for replies.
GCARR.1
GCARR.1Best answer
Visitor II
February 3, 2020

Well,

Let's take it back from the beginning/

(assuming XXXX is your version of CubeIDE)

1) install CubeIDE debian bundle:

sudo bash st-stm32cubeide_XXXX_amd64.deb_bundle.sh

2) you should get something like this:

dpkg -l "st-st*" "segger*"

Desired=Unknown/Install/Remove/Purge/Hold

| Status=Not/Inst/Conf-files/Unpacked/halF-conf/Half-inst/trig-aWait/Trig-pend

|/ Err?=(none)/Reinst-required (Status,Err: uppercase=bad)

||/ Name             Version       Architecture    Description

+++-============================-===================-===================-==============================================================

ii segger-jlink-udev-rules   6.62        all         segger-jlink-udev-rules

ii st-stlink-server       1.3.0-4       amd64        stlinkserver

ii st-stlink-udev-rules     1.0.2-2       all         st-stlink-udev-rules

ii st-stm32cubeide-XXXX amd64        IDE for STM32

3) Remove udev-rules-only segger package:

sudo dpkg -r --force-depends segger-jlink-udev-rules

4) Now you should have this:

dpkg -l "st-st*" "segger*"

Desired=Unknown/Install/Remove/Purge/Hold

| Status=Not/Inst/Conf-files/Unpacked/halF-conf/Half-inst/trig-aWait/Trig-pend

|/ Err?=(none)/Reinst-required (Status,Err: uppercase=bad)

||/ Name             Version       Architecture    Description

+++-============================-===================-===================-==============================================================

un segger-jlink-udev-rules   <none>       <none>       (no description available)

ii st-stlink-server       1.3.0-4       amd64        stlinkserver

ii st-stlink-udev-rules     1.0.2-2       all         st-stlink-udev-rules

ii st-stm32cubeide-XXXX amd64        IDE for STM32

CubeIDE is still there:

ls /opt/st/stm32cubeide_XXXX/stm32cubeide

artifacts.xml features      icon.xpm notice.html plugins stm32cubeide

configuration headless-build.sh jre    p2      readme  stm32cubeide.ini

5) install Segger JLink:

sudo dpkg -i JLink_Linux_V662a_x86_64.deb

(Reading database ... 239470 files and directories currently installed.)

Preparing to unpack JLink_Linux_V662a_x86_64.deb ...

Removing /opt/SEGGER/JLink ...

/opt/SEGGER/JLink not found (OK)

Unpacking jlink (6.621) ...

Setting up jlink (6.621) ...

6) Check what you have:

dpkg -l "st-st*" "segger*" "jlink*"

Desired=Unknown/Install/Remove/Purge/Hold

| Status=Not/Inst/Conf-files/Unpacked/halF-conf/Half-inst/trig-aWait/Trig-pend

|/ Err?=(none)/Reinst-required (Status,Err: uppercase=bad)

||/ Name             Version       Architecture    Description

+++-============================-===================-===================-==============================================================

ii jlink            6.621        amd64        SEGGER J-Link tools

un segger-jlink-udev-rules   <none>       <none>       (no description available)

ii st-stlink-server       1.3.0-4       amd64        stlinkserver

ii st-stlink-udev-rules     1.0.2-2       all         st-stlink-udev-rules

ii st-stm32cubeide-XXXX amd64        IDE for STM32

ls /opt/st/stm32cubeide_XXXX/

artifacts.xml features      icon.xpm notice.html plugins stm32cubeide

configuration headless-build.sh jre    p2      readme  stm32cubeide.ini

ls -l /etc/udev/rules.d/99-jlink.rules 

-rw-r--r-- 1 root root 20919 janv. 24 16:20 /etc/udev/rules.d/99-jlink.rules

Can you check this on your system?

Best regards.

4 replies

GCARR.1
Visitor II
January 31, 2020

Hello m4l490n,

To install  JLink_Linux_V662_x86_64.deb, you must first remove segger-jlink-udev-rules with the following command:

sudo dpkg -r --force-depends segger-jlink-udev-rules

This should not be an issue to run CubeIDE as segger-jlink-udev-rules only delivers /etc/udev/rules.d/99-jlink.rules which is also provided by JLink_Linux_V662.

Best regards.

m4l490n
m4l490nAuthor
Associate III
February 1, 2020

I can successfully install JLink_Linux_V662_x86_64.deb now with the suggested command but then STM32CubeIDE disappears. To install it again I have to uninstall JLink_Linux_V662_x86_64.deb and then I end up as in the beginning.

GCARR.1
GCARR.1Best answer
Visitor II
February 3, 2020

Well,

Let's take it back from the beginning/

(assuming XXXX is your version of CubeIDE)

1) install CubeIDE debian bundle:

sudo bash st-stm32cubeide_XXXX_amd64.deb_bundle.sh

2) you should get something like this:

dpkg -l "st-st*" "segger*"

Desired=Unknown/Install/Remove/Purge/Hold

| Status=Not/Inst/Conf-files/Unpacked/halF-conf/Half-inst/trig-aWait/Trig-pend

|/ Err?=(none)/Reinst-required (Status,Err: uppercase=bad)

||/ Name             Version       Architecture    Description

+++-============================-===================-===================-==============================================================

ii segger-jlink-udev-rules   6.62        all         segger-jlink-udev-rules

ii st-stlink-server       1.3.0-4       amd64        stlinkserver

ii st-stlink-udev-rules     1.0.2-2       all         st-stlink-udev-rules

ii st-stm32cubeide-XXXX amd64        IDE for STM32

3) Remove udev-rules-only segger package:

sudo dpkg -r --force-depends segger-jlink-udev-rules

4) Now you should have this:

dpkg -l "st-st*" "segger*"

Desired=Unknown/Install/Remove/Purge/Hold

| Status=Not/Inst/Conf-files/Unpacked/halF-conf/Half-inst/trig-aWait/Trig-pend

|/ Err?=(none)/Reinst-required (Status,Err: uppercase=bad)

||/ Name             Version       Architecture    Description

+++-============================-===================-===================-==============================================================

un segger-jlink-udev-rules   <none>       <none>       (no description available)

ii st-stlink-server       1.3.0-4       amd64        stlinkserver

ii st-stlink-udev-rules     1.0.2-2       all         st-stlink-udev-rules

ii st-stm32cubeide-XXXX amd64        IDE for STM32

CubeIDE is still there:

ls /opt/st/stm32cubeide_XXXX/stm32cubeide

artifacts.xml features      icon.xpm notice.html plugins stm32cubeide

configuration headless-build.sh jre    p2      readme  stm32cubeide.ini

5) install Segger JLink:

sudo dpkg -i JLink_Linux_V662a_x86_64.deb

(Reading database ... 239470 files and directories currently installed.)

Preparing to unpack JLink_Linux_V662a_x86_64.deb ...

Removing /opt/SEGGER/JLink ...

/opt/SEGGER/JLink not found (OK)

Unpacking jlink (6.621) ...

Setting up jlink (6.621) ...

6) Check what you have:

dpkg -l "st-st*" "segger*" "jlink*"

Desired=Unknown/Install/Remove/Purge/Hold

| Status=Not/Inst/Conf-files/Unpacked/halF-conf/Half-inst/trig-aWait/Trig-pend

|/ Err?=(none)/Reinst-required (Status,Err: uppercase=bad)

||/ Name             Version       Architecture    Description

+++-============================-===================-===================-==============================================================

ii jlink            6.621        amd64        SEGGER J-Link tools

un segger-jlink-udev-rules   <none>       <none>       (no description available)

ii st-stlink-server       1.3.0-4       amd64        stlinkserver

ii st-stlink-udev-rules     1.0.2-2       all         st-stlink-udev-rules

ii st-stm32cubeide-XXXX amd64        IDE for STM32

ls /opt/st/stm32cubeide_XXXX/

artifacts.xml features      icon.xpm notice.html plugins stm32cubeide

configuration headless-build.sh jre    p2      readme  stm32cubeide.ini

ls -l /etc/udev/rules.d/99-jlink.rules 

-rw-r--r-- 1 root root 20919 janv. 24 16:20 /etc/udev/rules.d/99-jlink.rules

Can you check this on your system?

Best regards.

m4l490n
m4l490nAuthor
Associate III
February 9, 2020

Awesome!! after following this I finally have both STM32CubeIDE and Segger JLink both working at the same time. I think the secret was to install JLink from the command line. Before, I was executing the same steps but double-clicking the .deb file to install JLink.