Question
Why are calls to strcat() not actually calling strcat()? (and why do I sometimes get a Hard Fault)
I am using STM32CubeIDE v1.6.1 and am seeing some strangeness.
When I call strcat(), I get a hardfault if the end of the string (where the nul is) being catted to is at an odd address?
Here is code from the .list file:
char s1[20];
strcpy(s1, "--");
800ab50: f107 030c add.w r3, r7, #12
800ab54: 4a65 ldr r2, [pc, #404] ; (800acec <sd_cmdproc_process_packet+0x374>)
800ab56: 6812 ldr r2, [r2, #0]
800ab58: 4611 mov r1, r2
800ab5a: 8019 strh r1, [r3, #0]
800ab5c: 3302 adds r3, #2
800ab5e: 0c12 lsrs r2, r2, #16
800ab60: 701a strb r2, [r3, #0]
strcat(s1, "1");
800ab62: f107 030c add.w r3, r7, #12
800ab66: 4618 mov r0, r3
800ab68: f7f5 fbc4 bl 80002f4 <strlen>
800ab6c: 4603 mov r3, r0
800ab6e: 461a mov r2, r3
800ab70: f107 030c add.w r3, r7, #12
800ab74: 4413 add r3, r2
800ab76: 495e ldr r1, [pc, #376] ; (800acf0 <sd_cmdproc_process_packet+0x378>)
800ab78: 461a mov r2, r3
800ab7a: 460b mov r3, r1
800ab7c: 881b ldrh r3, [r3, #0]
800ab7e: 8013 strh r3, [r2, #0]
strcat(s1, "2");
800ab80: f107 030c add.w r3, r7, #12
800ab84: 4618 mov r0, r3
800ab86: f7f5 fbb5 bl 80002f4 <strlen>
800ab8a: 4603 mov r3, r0
800ab8c: 461a mov r2, r3
800ab8e: f107 030c add.w r3, r7, #12
800ab92: 4413 add r3, r2
800ab94: 4957 ldr r1, [pc, #348] ; (800acf4 <sd_cmdproc_process_packet+0x37c>)
800ab96: 461a mov r2, r3
800ab98: 460b mov r3, r1
800ab9a: 881b ldrh r3, [r3, #0]
800ab9c: 8013 strh r3, [r2, #0]
800ab9e: e1c4 b.n 800af2a <sd_cmdproc_process_packet+0x5b2>
}the strcat of "1" works, but the strcat of "2" hard faults. I suspect it isalignment error with the "strh".
It is also curious that the calls to strcat() (and strcpy()) do not call the actual functions.
I appologize if I have missed something obvious.
Thanks,
mark