Skip to main content
KBéla.1
Associate III
August 27, 2020
Question

Which is the highest frequency signal that the SWV Data Trace Timeline graph can show?

Hello, I trying to trace audio signal by SWV Data Trace Timeline graph? I cant do it. I can show normally only 10Hz signal. Higher frequency signals make a mismatch in timeline graph. I m using STM32F769 mcu, with coreClock: 216Mhz, SWO Clock: 2000kHz in CubeIDE 1.2.1 environment with an original ST-Link/V2 debugger.

I m trying to show the values of a global variable.

Thank you in advance.

This topic has been closed for replies.

1 reply

Visitor II
January 30, 2024

I too am having same issue, if anyone can address the solution. My thinking goes toward the limited baudrate of UART.