When I use c++, and I modify .iot file, it doesn't generate the code anymore
To use cpp, I create the project in cpp and then I modify the name of main.c in main.cpp. This work pretty well, but when I try to update the configuration by ioc file, the code stay the same. It seems like I have to change to main.c before update to be fine. Do it exists a more easy way without modify the main extension everytime? Ty