What is the most effective way for using assembly code at the core of interrupt handling?
I've been able to successfully handle my tasks via C using the interrupt entry for DMA1_Stream0_IRQHandler() but want to rewrite it in assembly code (let's please not get into a discussion of whether this is worth it or not for performance reasons).
When trying to write pure assembly code, I see STMCubeIDE offer me only C or C++ source files, apparently nothing for ASM. What's an effective way to do it then? I specifically want to write code that is called when the interrupt for DMA1_Stream0_IRQHandler() is called.
Some hints in the right direction or even some simple framework would be highly appreciated. I can take it from there. So far I haven't really had much luck to find instructions on the internet.