Question
What is the best way to enable Debug messages for USB Host?
After selecting the USBH_DEBUG_LEVEL option with a value of 3 (Middleware > Parameter Settings > USBH_DEBUG_LEVEL) and adding these subroutines below (BEGIN 4 / END 4), the messages have not yet been displayed on the serial monitor. Only after adding a message (BEGIN 2 / END 2) in the main routine the Debug messages were displayed correctly.
(main.c file:)
/* USER CODE BEGIN 4 */
int __io_putchar(int ch) {
uint8_t c[1];
c[0] = ch & 0x00FF;
HAL_UART_Transmit(&huart1, &*c, 1, 10);
return ch;
}
int _write(int file, char *ptr, int len) {
int DataIdx;
for (DataIdx = 0; DataIdx < len; DataIdx++) {
__io_putchar(*ptr++);
}
return len;
}
/* USER CODE END 4 */(main.c file:)
int main(void)
{
...
/* USER CODE BEGIN 2 */
USBH_UsrLog("Power On"); // <--------------- ???
/* USER CODE END 2 */This happens from version 1.0 to version 1.4 of the STM32CubeIDE !?