Skip to main content
Jim Seymour
Senior
Mar 10, 2026 7:05 PM UTC
Solved

What if I *want* a LOAD segment with RWX permissions?

I'm getting the "elf has a LOAD segment with RWX permissions" warning, and a quick search here reveals a couple of ways to get around this: Disable the warning, or edit the .ld file.

However, in my case, I'm using the upper half of the STM32's flash area to emulate non-volatile memory.  So I want my flash to be writeable.

Can anyone suggest some magic to put in my linker file that will make the warning go away, but also allow me to write to flash?

Also: I'm using STM32CubeIDE, so my linker file is auto-generated.  Is there a user-override mechanism (like there is in the source code)?

Thanks.

mfgkwBest answer
Associate II
Mar 10, 2026 7:26 PM UTC

But the part you write will probably have no code?

Then you can split the flash in two parts: rx for the code and rw for your data.

 

So if you have something like:

MEMORY
{
 RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 512K
 FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 2048K
}

change it to e.g.:

MEMORY
{
 RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 512K
 FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 1024K
 FLASHEMU (rw) : ORIGIN = 0x8100000, LENGTH = 1024K
}

(untested, just a proposal)

3 replies

mfgkwBest answer
Associate II
Mar 10, 2026 7:26 PM UTC

But the part you write will probably have no code?

Then you can split the flash in two parts: rx for the code and rw for your data.

 

So if you have something like:

MEMORY
{
 RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 512K
 FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 2048K
}

change it to e.g.:

MEMORY
{
 RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 512K
 FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 1024K
 FLASHEMU (rw) : ORIGIN = 0x8100000, LENGTH = 1024K
}

(untested, just a proposal)

Jim Seymour
Senior
Mar 11, 2026 4:28 PM UTC

Thanks. Now that I think this problem through, this solves an issue I was worried about: My code overflowing the first half of flash.

It doesn't solve the warning issue.  But on further research, it seems that the only way to get around that is to suppress it.  This is because I'm using the hal_flash routines - and one of them is declared with __RAM_FUNC (which puts it in the RAM segment - which is rwx).

 

Pavel A.
Mar 11, 2026 2:38 AM UTC

> So I want my flash to be writeable.

From the linker POV this memory is still not-writeable, so just leave the linker file as is. No change is needed.

If you like, divide the FLASH region as @mfgkw proposed, (with r attribute) - only for convenience, to ensure that the program fits in the reduced FLASH size.