Skip to main content
Iviti.1
Associate II
November 23, 2020
Question

What exactly starts the clk during spi communications?

According to section 28.9.1 (of RM0091), the spi communications are enabled when register 6 is active (SPE set to 1). According to the rm0091 guide, once the spi communications are active, and register 14 is set to 0 (receive only mode) then the clk pin should start up. But when I pause the debugger at that stage, I can see both those pins be in the correct setting, but sometimes the clock is on and sometimes it is not on. So what exactly starts the clk during spi communications?

I dont know if it matters, but I am connected in half duplex master mode to an spi compatible chip (ssc). I am using an stm32f042k6t6 chip on a nucleo board.

This topic has been closed for replies.

12 replies

Nikita91
Lead II
November 23, 2020

What means "register 6 is active" ? You mean SPE bit in CR1 register ?

The clock starts when something is written in the DR register and stops at the end of this data transmission.

Iviti.1
Iviti.1Author
Associate II
November 23, 2020

I disagree that the clock starts when something is written in the DR register, at least during the receive stage. on line 1072 of stm32f0xx_hal_spi.c, it states:

 if ((hspi->Instance->CR1 & SPI_CR1_SPE) != SPI_CR1_SPE)
 
 {
 
 /* Enable SPI peripheral */
 
 __HAL_SPI_ENABLE(hspi);
 
 }

In other words , check if spi is enabled, if it's not, then enable it. But If I remove the "if" section and just tell it to enable spi no matter what, then it starts the clock at that point. Yet I have not started writing to the dr register. Also, on receive, the external (slave) chip doesnt know to start sending until clk is active.

waclawek.jan
Super User
November 23, 2020

Read out and check/post the SPI registers content just before that line.

JW

Iviti.1
Iviti.1Author
Associate II
November 24, 2020

the contents of CR1 are 1000001101011101

Where the 14th bit is 0 (receive mode) and the 6th bit is 1 (SPI active)

Nikita91
Lead II
November 24, 2020

As the clock runs only when the master has something to transmit, check if the TX FIFO is empty when you enable the SPI setting SPE bit.

Iviti.1
Iviti.1Author
Associate II
November 24, 2020

If the clock only runs when master needs to transmit, how does it receive messages? In other words, how does the slave transmit with no clock?

waclawek.jan
Super User
November 24, 2020

And other SPI registers?

CR1 appears to be OK, there may be some internal state though which prevents the clocks, to which it arrived through previous history; so we need to know about that history. Maybe there's also some hardware dependency.

Please prepare a minimal but complete compilable example exhibiting the problem; best without using any "library" such as Cube.

JW

PS. @Nikita91​ , the SPI is here set to bidirectional mode (halfduplex, CR1.BIDIMODE=1), when you turn it into Rx, it ought to clock automatically.

Iviti.1
Iviti.1Author
Associate II
November 24, 2020

Ok, So I checked all of the spi registers (cr1,cr2,sr,both i2c, and all 3 crc). Only CR1 changes between cycles:

  1. CR1 = 831d (spe off, receive mode)
  2. hal transmit
  3. CR1 = c35d (spe on, send mode)
  4. hal receive
  5. CR1 = 835d (spe on, receive mode)
  6. (next cycle)
  7. CR1 = 835d (spe on, receive mode)
  8. hal transmit
  9. CR1 = c35d (spe on, send mode)
  10. hal receive
  11. CR1 = 831d (spe off, receive mode)
  12. (start over)

What is strange is that before we go into receive mode both times, all of the registers are in the exact same states. Yet in one cycle, it remembers to turn on the CLK and the other one it does not.

Ill work on a minimal example, but it's as minimal as it gets (hal spi transmit, then hal spi receive). Delays if you want them but they dont change anything.

waclawek.jan
Super User
November 24, 2020

I don't use Cube/HAL so you may perhaps extract the relevant lines from it and insert it into your code directly.

JW

Iviti.1
Iviti.1Author
Associate II
November 25, 2020

I keep reading that people avoid cube/hal. Is it that buggy?

waclawek.jan
Super User
November 25, 2020

It of course has its own share of bugs, but generally I don't think it's more buggy than any other software.

I don't use Cube/HAL - nor Cube/LL or SPL, for that matter - because I don't think it brings any benefit to me. I can read the manual and program accordingly. Would I use a "library", I would need to learn that library - and in the case of problem I would need to learn the real stuff anyway, so that's double work.

With Cube/HAL, there's one more thing which deters me. It tries to be relatively "smart". But doing so, it inevitably limits itself to the "most common usage modes", as it's impossible to be "smart" in every conceivable way a user wants to use the mcu and its features - there are simply too many, as you try to combine the already massive amount of features with the many ways how to use them. In other words, while doing "ordinary" things, Cube/HAL may be an immense help; but as soon as you try to do something "out of ordinary", Cube/HAL may start to be less helpful or even straight get into your way.

YMMV

JW

Nikita91
Lead II
November 26, 2020

I follow this opinion about HAL.

But I often use LL because the most interesting parts are:

  • naming each bit of each register with a clear name (this can be seen as a complement to the CMSIS MCU description file)
  • Macros for set / reset each bits with a clear name. And some nice functions to initialize devices.

This gives a clearer and practically commented code.