Skip to main content
Associate II
Nov 7, 2025 10:13 AM UTC
Solved

Warning: macOS update to 26.1 breaks Eclipse text selection

Hello,

if you are using macOS and STM32CubeIDE and need it productively you should currently refrain updating your macOS. Due to a bug in Eclipse (https://github.com/eclipse-platform/eclipse.platform.swt/issues/2621) text selection does no more work via dragging your mouse or using shift+arrows.

There is already a fix but STM32CubeIDE does not provide the fix as update as of now.

I already filed a case. 

Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
Nov 7, 2025 2:00 PM UTC

Hello @st_otto 

In the meantime, STM32CubeIDE 1.19.0 is not supported on macOS 26.1, according to release note RN0114.

GhofraneGSOURI_0-1762523959053.png

 

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

20 replies

grisom13
Associate III
Jan 8, 2026 7:57 PM UTC

rework crash the app. Tahoe 26.2  CubeIDE 1.19.0

Andrei Chichak
Lead
Jan 8, 2026 8:13 PM UTC

Bug observed in MacOS 26.2 with CubeIDE 2.0.0 as well.

And Eclipse 2025-06 (4.36.0).

To be fair (asking a lot) this is not an ST problem. Both Eclipse and CubeIDE worked properly prior to updating to MacOS 26.2. The people that complain that ST should be better at choosing when to release a system should remember that Apple radically changed how their UI works, ultimately breaking Eclipse and CubeIDE. This is also not the first time that Apple's alterations borked Eclipse and CubeIDE, don't you remember the upside-down splash screen? That was corrected by Eclipse AND Apple subsequently.

So, hang on for a while and fixes will be coming.

BTW, control-space code completion doesn't work too.

grisom13
Associate III
Jan 8, 2026 11:03 PM UTC

UPD. Works fro me now. For some reason copy pasting filename make some autocorrections and changed ","  to "_"

 

 

Associate
Mar 15, 2026 3:43 PM UTC

i am using the latest STM32CubeIDE v 2.1.0

on an apple silicon macos

 

I did what was written in one of the previous posts. It is not working.

There is a log file generated.

I created an screendump attached.

I am not sure what is wrong.

Anyone any idea?

Associate
Mar 15, 2026 3:45 PM UTC

It is a really annoying bug. Especially when copying and pasting. You have no clue what has been selected.

 

I will remove the ide and reinstall since i changed something and it will not start anymore.

Graduate
Apr 16, 2026 3:16 PM UTC

I just ran into the same problem after a forced MacOS upgrade.

IDE 2.1.1

MacOS 26.4.1

Apple M4 Pro

I hope a solution is in the works. Rolling back does not seem to be an option.

Marcelo Barros
Associate III
Aug 1, 2026 12:59 PM UTC

I tried this solution on my Mac (M2 Pro, Tahoe 26.5.2), but it didn't work. The filenames were related to aarch64, not x86.

 

Mac files:

org.eclipse.swt_3.127.0.v20240903-0618.jar
org.eclipse.swt.cocoa.macosx.aarch64_3.127.0.v20240903-0618.jar

 

Downloaded eclipse files

org.eclipse.swt_3.132.0.v20251124-0642.jar

org.eclipse.swt.cocoa.macosx.aarch64_3.132.0.v20251124-0642.jar

 

I fixed the file names inside bundles.info but Cube IDE always report an error.
 

ST could give more attention to this problem.

I know Tahoe is listed as not supported but macos users are stopping using cube ide tool.