Skip to main content
Associate
September 24, 2024
Solved

VERY weird 'Failed to execute MI command' problem

Hi everyone,
 
I start to question myself and this whole programming thing....
 
I'm using a STM32F3-Discovery Board and generated a code with STM32CubeMX in default mode. I changed absolutely nothing before code generation.
 
In main.c I added the following code to the default one:
 
#include "math.h"
#define PI 3.141
uint32_t sine_val[100];
 
void calcsin(void){
        for (int i=0; i<100; i++) {
        sine_val[i] = ((sin(i*2*PI/100) + 1)*(4096/2));
       }
}
 
That's all. So nothing special at all. The thing is, everything is fine but whenever I try to call calcsin() in the int main function I get the following error:
 
Error in final launch sequence:
 
Failed to execute MI command:
load E:\\STM32\\Workspace\\090924\\Default\\Debug\\Default.elf 
 
Error message from debugger back end:
Error finishing flash operation
 
Also the STM32CubeIDE opens another error message (sporadically?!) which says "No source available for "__muldf3() at 0x8000754"
 
Can somebody please help? 

 

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
September 24, 2024

Hello @RedScorpio95 and welcome to the community.

I didn't reproduce the behavior on STM32F3-Discovery board.

Attached a project. Could you please double check?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
September 24, 2024

Hello @RedScorpio95 and welcome to the community.

I didn't reproduce the behavior on STM32F3-Discovery board.

Attached a project. Could you please double check?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.