Skip to main content
Associate II
February 24, 2024
Solved

Utilizing a 512Mbit SDRAM with STM32H7 FMC

Hello everyone,

I'm working on a project involving STM32's FMC specifically focusing on expanding memory capabilities. Given that each SDRAM bank (Bank 1 and Bank 2) can address up to 256 Mbit, I'm curious about the feasibility of integrating a single SDRAM chip with a larger capacity, specifically a 512Mbit chip with 13 address lines, such as the one detailed here: 

https://www.issi.com/WW/pdf/42-45R-S-32160F.pdf

Is there a method or configuration within the STM32 FMC that would allow me to effectively use all of the 512Mbit SDRAM's capacity? or I have to use two 256Mbit SRAM with the individual clock and chip enable controls. Any insights or guidance on this would be greatly appreciated.

Thank you in advance for your assistance.

 

    This topic has been closed for replies.
    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    February 24, 2024

    The address window is 256 MB(yte) not 256 Mb(it)

    512Mb == 64MB

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

    2 replies

    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    February 24, 2024

    The address window is 256 MB(yte) not 256 Mb(it)

    512Mb == 64MB

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Associate II
    February 24, 2024

    That was a silly mistake. Thank you!