Skip to main content
Clark Sann
Associate III
Mar 30, 2025 1:16 AM UTC
Question

Using Python virtual environment in Cube IDE

I am developing an SBSFU based project for the B-U585I-IOT02A discovery board. The SBSFU project contains various python scripts that are automatically run during the build process. 

How can I force STM32CubeIDE to use the Python version and packages in my virtual environment? 

This topic has been closed for replies.

1 reply

Pavel A.
Mar 30, 2025 3:57 PM UTC

To force python to use a specific venv, make sure that the python binary is the one inside the venv. Modify the PATH or do whatever else.