Skip to main content
Visitor II
May 21, 2024
Solved

USBPD for STM32L562

Hi ,

      I was given by a task to connect an external load to STM32L562 for USBPD. Do you guys have any idea how to start and what to do in the inital process.

 

Task details 

Support all 100W+ USB PD EPR power profiles using standard USB PD 3.1 parameters, 100W (20V @ 5A),  140W (28V @ 5A) , 180W (36V @ 5A) , 240W (48V @ 5A).  240W may not be able to be tested during this phase due to market availably of OTS 240W supplies, however functionality should be added for future use
Requires an external load on the module connectors to validate power delivery output capability

 

    This topic has been closed for replies.
    FBLBest answer
    ST Technical Moderator
    May 21, 2024

    Hi @nishadh 

    TCPP upgrade to support EPR voltages is ongoing ;)

    For further details, check this thread Solved: Re: USB PD sink - STMicroelectronics Community

    To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL

    1 reply

    FBLBest answer
    ST Technical Moderator
    May 21, 2024

    Hi @nishadh 

    TCPP upgrade to support EPR voltages is ongoing ;)

    For further details, check this thread Solved: Re: USB PD sink - STMicroelectronics Community

    To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL