Skip to main content
S.Ma
Principal
March 21, 2020
Question

Upgrading CubeIDE 1.2 to 1.3 fails

  • March 21, 2020
  • 3 replies
  • 1355 views

I could download latest HAL library for STM32L4 (which means my internet setup maybe correct), but when trying to launch an upgrade to CubeIDE 1.3, it fails (no upgrade available, server unavailable). Is it just me? (no apparent related post found so far) or should I just download a full install of 1.3 ?

This topic has been closed for replies.

3 replies

S.Ma
S.MaAuthor
Principal
March 21, 2020

Installing Cube3.0 took 5 mn to download the 0.7GB zip files, 3 minutes to install, then about 15mn to figure out how to migrate from Cube 1.2 project into Cube 1.3

Build seems ok, now need to check if the SW still does the same thing as HAL version changed too.

Julien D
ST Employee
March 23, 2020

Hello Dot,

About your upgrade issue, may I ask you if you are behind a proxy ?

If so, did you configured it in [ Preferences > Network Connections ] ?

In fact I also experienced this by settings the 3 protocols (HTTP, HTTPS, SOCKS); it works well if I set only HTTP(S) and let SOCKS empty, but only when restarting STM32CubeIDE or reloading manually all the sites urls from [ Preferences > Install/Update > Available Software Sites ] after each proxy settings changes.

HTH

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
S.Ma
S.MaAuthor
Principal
March 23, 2020

I was able to use CubeIDE to download the latest HAL but upgrading CubeIDE failed. Network connection was ok (as I could update HAL), network connections as DIRECT. Installing from scratch was faster than trying to upgrade. Importing 1.2 project into 1.3 was the only main challenge here.