Unwanted interaction between CubeIDE and CubeMX
I'm working on some code in CubeIDE but need some settings from another project. I have two choices, I can keep switching between .ioc files (which doesn't work well since I can't have both open at the same time), or I can fire up CubeMX on the other project and nicely scroll through the things I need.
BUT (a big but), there's a problem. With project B open in CubeMX, if I try and open the .ioc file for project A in CubeIDE, CubeIDE will bring up the project chooser screen instead of just opening the .ioc file that I clicked on.
My system is an Intel Mac, MacOS latest, CubeIDE latest, CubeMX latest.