Skip to main content
Kaveh
Associate III
November 1, 2020
Solved

unknown type name 'TIM_HandleTypeDef'; did you mean 'I2C_HandleTypeDef'?

Hello,

I just created a CubeMX project and tried to create a timer handler/ I am getting bellow error.

../Src/main.c:46:1: error: unknown type name 'TIM_HandleTypeDef'; did you mean 'I2C_HandleTypeDef'?

 TIM_HandleTypeDef htimer2;

Here is the code:

 
#include "main.h"
#include "stm32h7xx_hal.h"
 
 
 
 
UART_HandleTypeDef huart2;
TIM_HandleTypeDef htimer2;
 
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART2_UART_Init(void);
void GPIO_Init(void);
void LSE_Config(void);
 
 
char *data = "Hello world, I made it using STM32 ARM Cortex M7!\r\n";
 
 
 
int main(void)
{
 
 HAL_Init();
 SystemClock_Config();
 MX_GPIO_Init();
 GPIO_Init();
 MX_USART2_UART_Init();
 
	char msg[100];
	char *user_data = "Hello world, I made it using STM32 ARM Cortex M7!\r\n";
 	if (HAL_UART_Transmit(&huart2,(uint8_t*)user_data,strlen(user_data), HAL_MAX_DELAY) != HAL_OK)
 	{
 		// Error occurred
 		Error_Handler();
 	}
 
 
 
 
 	while(1);
 
 
 
	data = "End of program\r\n";
	HAL_UART_Transmit(&huart2,(uint8_t*)data,strlen(data), HAL_MAX_DELAY);
}
 
/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
 
 /** Supply configuration update enable
 */
 HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
 /** Configure the main internal regulator output voltage
 */
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
 
 while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 //RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
 |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
 RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV1;
 RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
 {
 Error_Handler();
 }
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USART2;
 PeriphClkInitStruct.Usart234578ClockSelection = RCC_USART234578CLKSOURCE_D2PCLK1;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
}
 
/**
 * @brief USART2 Initialization Function
 * @param None
 * @retval None
 */
static void MX_USART2_UART_Init(void)
{
 
 /* USER CODE BEGIN USART2_Init 0 */
 
 /* USER CODE END USART2_Init 0 */
 
 /* USER CODE BEGIN USART2_Init 1 */
 
 /* USER CODE END USART2_Init 1 */
 huart2.Instance = USART2;
 huart2.Init.BaudRate = 115200;
 huart2.Init.WordLength = UART_WORDLENGTH_8B;
 huart2.Init.StopBits = UART_STOPBITS_1;
 huart2.Init.Parity = UART_PARITY_NONE;
 huart2.Init.Mode = UART_MODE_TX_RX;
 huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart2.Init.OverSampling = UART_OVERSAMPLING_16;
 huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart2.Init.ClockPrescaler = UART_PRESCALER_DIV1;
 huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&huart2) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetTxFifoThreshold(&huart2, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetRxFifoThreshold(&huart2, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_DisableFifoMode(&huart2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART2_Init 2 */
 
 /* USER CODE END USART2_Init 2 */
 
}
 
/**
 * @brief GPIO Initialization Function
 * @param None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 
 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 
}
 
 
void GPIO_Init(void)
{
	__HAL_RCC_GPIOD_CLK_ENABLE();
	GPIO_InitTypeDef ledgpio;
	ledgpio.Pin = GPIO_PIN_14;
	ledgpio.Mode = GPIO_MODE_OUTPUT_PP;
	ledgpio.Pull = GPIO_NOPULL;
	HAL_GPIO_Init(GPIOD, &ledgpio);
}
/* USER CODE BEGIN 4 */
 
/* USER CODE END 4 */
 
/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
	data = "Something went wrong\r\n";
	HAL_UART_Transmit(&huart2,(uint8_t*)data,strlen(data), HAL_MAX_DELAY);
	while(1)
	{
		HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_14);
	}
}
 
void LSE_Config(void)
{
	RCC_OscInitTypeDef OSC_Init;
 
	// Activating LSE
	OSC_Init.OscillatorType = RCC_OSCILLATORTYPE_LSE;
	OSC_Init.LSEState = RCC_LSE_ON;
	if (HAL_RCC_OscConfig(&OSC_Init) != HAL_OK)
	{
		Error_handler();
	}
 
	// Configuring LSE to input pin
	HAL_RCC_MCOConfig(RCC_MCO1,RCC_MCO1SOURCE_LSE,RCC_MCODIV_1);
}
 
#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @param file: pointer to the source file name
 * @param line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
 
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

This topic has been closed for replies.
TDK
TDKBest answer
November 2, 2020

Seems like the timer was not active when you generated the CubeMX code and you added it afterwards. Seems like you modified the main() function quite a bit as well.

You can go into the stm32*_hal_conf.h file and activate the timer module (#define HAL_TIM_MODULE_ENABLED). Or you can regenerate the CubeMX with the timer activated.

"If you feel a post has answered your question, please click ""Accept as Solution""."

4 replies

TDK
TDKBest answer
November 2, 2020

Seems like the timer was not active when you generated the CubeMX code and you added it afterwards. Seems like you modified the main() function quite a bit as well.

You can go into the stm32*_hal_conf.h file and activate the timer module (#define HAL_TIM_MODULE_ENABLED). Or you can regenerate the CubeMX with the timer activated.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Visitor II
January 24, 2024

Hi, TDK i try to enabled already but why i got this error " Description Resource Path Location Type
fatal error: stm32g0xx_hal_tim.h: No such file or directory stm32g0xx_hal_conf.h /X590-MB-G071KBU6/Core/Inc line 316 C/C++ Problem"

TDK
January 24, 2024

It sounds like the file doesn't exist at the specified location. Does it?

Please open a new thread with relevant information instead of re-posting in this one as your issue is not the same, and this thread is solved.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Kaveh
KavehAuthor
Associate III
November 2, 2020

Yes, you guessed it right. The timer was not active and worked just fine after uncommenting #define HAL_TIM_MODULE_ENABLED.

Also, I am in the learning phase, that's why main() is modified so much.

Thanks for the quick help!