Skip to main content
SnoZek
Associate III
Nov 28, 2023 8:02 AM UTC
Solved

Unit Testing STM32

Hello everyone,

I'm posting here because I have an issue in my project. We've developed a board with an STM32 processor, and I would like to perform hardware tests on one side (not difficult so far) and, on the other side, be able to execute purely software unit tests without the need to use the board (doing everything on PC).

My code uses a structure that encapsulates all the hardware functions in a specific file. I've attempted to use a different compiler from cubeIDE to execute code directly on the PC, as described here:

https://michael.kafarowski.com/blog/unit-testing-with-stm32cubeide/

It works well for very simple code. I've tried using the cmock tool to simulate my hardware part, but I always encounter inclusion problems.

Has anyone successfully achieved abstraction hardware part? Could you provide me with some advices?

Thank you, Yvan

 

This topic has been closed for replies.
Michael K
Michael KBest answer
Senior III
Dec 5, 2023 11:16 PM UTC

When you say "inclusion problems" I assume you're referring to trying to import and unit test parts of the STM32 HAL. My article mainly focused on unit testing business logic that sits above the hardware abstraction layer. The example I used the article is trivial of course. Perhaps I should have included a more comprehensive example to make that point more clear.

A case in which I've used unit testing in practice was with an interface for UART communication. On the real device, the interface implementation would receive characters and send them through to the STM32 HAL or into an RTOS queue. Because the interface was loosely coupled, I could use the interface to implement a Spy which processes those characters and confirms them against unit tests. 

In this case the intention was to isolate and test the business logic all the way down to the characters that would be sent over the UART, while ignoring the queue or the HAL. Testing the queue or HAL would have meant testing on the target or using complex simulators - in either case, the cycle time of tests would have been very long. In comparison, running the tests of the business logic as I described above took less than a second and could be done frequently throughout development to catch bugs before they're covered up.

As you've discovered, unit testing may not be the optimal solution for testing closer to the hardware, but it's a valuable tool in testing other parts of your application. Testing business logic in isolation removes the doubt of the hardware element as it relates to the business logic itself. Other types of tests more specific to hardware would be valuable as well.

Embedded UI/UX Consulting: cadenza.design

1 reply

Michael K
Michael KBest answer
Senior III
Dec 5, 2023 11:16 PM UTC

When you say "inclusion problems" I assume you're referring to trying to import and unit test parts of the STM32 HAL. My article mainly focused on unit testing business logic that sits above the hardware abstraction layer. The example I used the article is trivial of course. Perhaps I should have included a more comprehensive example to make that point more clear.

A case in which I've used unit testing in practice was with an interface for UART communication. On the real device, the interface implementation would receive characters and send them through to the STM32 HAL or into an RTOS queue. Because the interface was loosely coupled, I could use the interface to implement a Spy which processes those characters and confirms them against unit tests. 

In this case the intention was to isolate and test the business logic all the way down to the characters that would be sent over the UART, while ignoring the queue or the HAL. Testing the queue or HAL would have meant testing on the target or using complex simulators - in either case, the cycle time of tests would have been very long. In comparison, running the tests of the business logic as I described above took less than a second and could be done frequently throughout development to catch bugs before they're covered up.

As you've discovered, unit testing may not be the optimal solution for testing closer to the hardware, but it's a valuable tool in testing other parts of your application. Testing business logic in isolation removes the doubt of the hardware element as it relates to the business logic itself. Other types of tests more specific to hardware would be valuable as well.

Embedded UI/UX Consulting: cadenza.design