Skip to main content
Renato Valentim
Associate III
Mar 12, 2020 6:35 PM UTC
Solved

undefined reference to HAL_TIM* functions

I'm having a problem where the linked complains to me with undefined reference to `HAL_TIM_PWM_Init' erros. The objects that it complains are not defined are HAL TIM based ones such as HAL_TIM_PWM_Init or HAL_TIM_IRQHandler. There is a source file with these functions defined that is compiled "stm32f7xx_hal_tim.c" but for some reason the linker still complains.

Here is some source code (the last line gives me the error):

#include <string.h>
#include "stm32f7xx_hal.h"
#include "stm32f7xx_hal_tim.h"
#include "ws2812b.h"
 
extern WS2812_Struct ws2812b;
 
// Define source arrays for my DMAs
uint32_t WS2812_IO_High[] = { WS2812B_PINS };
uint32_t WS2812_IO_Low[] = {WS2812B_PINS << 16};
 
// WS2812 framebuffer - buffer for 2 LEDs - two times 24 bits
uint16_t ws2812bDmaBitBuffer[24 * 2];
 
// Gamma correction table
const uint8_t gammaTable[] = {
 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0,
 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 1, 1, 1, 1,
 1, 1, 1, 1, 1, 1, 1, 1, 1, 2, 2, 2, 2, 2, 2, 2,
 2, 3, 3, 3, 3, 3, 3, 3, 4, 4, 4, 4, 4, 5, 5, 5,
 5, 6, 6, 6, 6, 7, 7, 7, 7, 8, 8, 8, 9, 9, 9, 10,
 10, 10, 11, 11, 11, 12, 12, 13, 13, 13, 14, 14, 15, 15, 16, 16,
 17, 17, 18, 18, 19, 19, 20, 20, 21, 21, 22, 22, 23, 24, 24, 25,
 25, 26, 27, 27, 28, 29, 29, 30, 31, 32, 32, 33, 34, 35, 35, 36,
 37, 38, 39, 39, 40, 41, 42, 43, 44, 45, 46, 47, 48, 49, 50, 50,
 51, 52, 54, 55, 56, 57, 58, 59, 60, 61, 62, 63, 64, 66, 67, 68,
 69, 70, 72, 73, 74, 75, 77, 78, 79, 81, 82, 83, 85, 86, 87, 89,
 90, 92, 93, 95, 96, 98, 99,101,102,104,105,107,109,110,112,114,
 115,117,119,120,122,124,126,127,129,131,133,135,137,138,140,142,
 144,146,148,150,152,154,156,158,160,162,164,167,169,171,173,175,
 177,180,182,184,186,189,191,193,196,198,200,203,205,208,210,213,
 215,218,220,223,225,228,231,233,236,239,241,244,247,249,252,255 };
 
static void ws2812b_gpio_init(void)
{
	// WS2812B outputs
	WS2812B_GPIO_CLK_ENABLE();
	GPIO_InitTypeDef GPIO_InitStruct;
	GPIO_InitStruct.Pin = WS2812B_PINS;
	GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
	GPIO_InitStruct.Pull = GPIO_NOPULL;
	GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
	HAL_GPIO_Init(WS2812B_PORT, &GPIO_InitStruct);
 
	// Enable output pins for debuging to see DMA Full and Half transfer interrupts
	#if defined(LED4_PORT) && defined(LED5_PORT)
		GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
		GPIO_InitStruct.Pull = GPIO_NOPULL;
		GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
 
		GPIO_InitStruct.Pin = LED4_PIN;
		HAL_GPIO_Init(LED4_PORT, &GPIO_InitStruct);
		GPIO_InitStruct.Pin = LED5_PIN;
		HAL_GPIO_Init(LED5_PORT, &GPIO_InitStruct);
	#endif
}
 
TIM_HandleTypeDef Tim2Handle;
TIM_OC_InitTypeDef tim2OC1;
TIM_OC_InitTypeDef tim2OC2;
 
uint32_t tim_period;
static void TIM2_init(void)
{
	// TIM2 Periph clock enable
	__HAL_RCC_TIM2_CLK_ENABLE();
 
	// This computation of pulse length should work ok,
	// at some slower core speeds it needs some tuning.
	tim_period = SystemCoreClock / 800000; // 0,125us period (10 times lower the 1,25us period to have fixed math below)
	uint32_t cc1 = (10 * tim_period) / 36;
	uint32_t cc2 = (10 * tim_period) / 15;
 
	Tim2Handle.Instance = TIM2;
 
	Tim2Handle.Init.Period = tim_period;
	Tim2Handle.Init.RepetitionCounter = 0;
	Tim2Handle.Init.Prescaler = 0;
	Tim2Handle.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
	Tim2Handle.Init.CounterMode = TIM_COUNTERMODE_UP;
	HAL_TIM_PWM_Init(&Tim2Handle);
 

Any ideas?

Thanks!

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Mar 12, 2020 8:30 PM UTC

Make sure to enable TIM functions in stm32f7xx_hal_conf.h

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

5 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Mar 12, 2020 8:30 PM UTC

Make sure to enable TIM functions in stm32f7xx_hal_conf.h

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
dbgarasiya
Senior
Mar 13, 2020 5:03 AM UTC

have you enable timer

Renato Valentim
Associate III
Mar 13, 2020 10:40 AM UTC

I enabled the timer through the stm32f7xx_hal_conf.h. It works now! Thanks!!!!!

Associate
Sep 24, 2024 3:56 PM UTC

newbie here with same problem .. playing with example code 

how did u enable the timer ? 

dbgarasiya
Senior
Mar 13, 2020 11:46 AM UTC

great