Skip to main content
Agour.1
Associate III
June 29, 2022
Solved

Unbale to connect to the network

  • June 29, 2022
  • 19 replies
  • 10639 views

We want to migrate from STM32L4+ to STM32U5 series of processor.. this latest software is not supported by older ide (1.6.0) so we need to migrate from stm32cubeide 1.6.0 to 1.10.0..

I have un-installed the older version and cleared all possible directories, disabled firewall, and removed antivirus. we are using windows7 OS.

Done appropriate proxy settings in Window-->Preferences-->Network Connections as per https://wiki.st.com/stm32mpu/wiki/How_to_set_up_proxy_and_P2P_Ethernet_connection_with_STM32CubeIDE.

Upon checking connection status in Window-->Preferences-->STM32Cube-->Firmware updater the check connection failure is noticed. I am unable to create any STM32 project as it needs a network connection for downloading the repository.

I am able to connect properly to another computer in our LAB. with the above-given procedures.

Kindly let me know pointers to debug this issue further.

0693W00000Nt3U1QAJ.png0693W00000Nt3OGQAZ.png

This topic has been closed for replies.
Best answer by Aymen CHAKROUN

Hi @Agour.1​ ,

I'm suspecting a certificate issue with your proxy company.

The other PC Lab (where CubeIDE execution is OK), is also running on Windows 7 ?

Last trial to test:

  • Open the file "C:\ST\STM32CubeIDE_1.10.0\STM32CubeIDE\stm32cubeide.ini"
  • Remove the line -Djavax.net.ssl.trustStoreType=WINDOWS-ROOT
  • Delete your "C:\Users\<usename>\STM32CubeIDE" workspace
  • Delete .eclipse and .stm32cubemx folders
  • Retry to open CubeIDE, setup your usual manual proxy and perform a test connection (may be do the check twice)

Regards,

Aymen.

19 replies

Markus GIRDLAND
ST Employee
June 30, 2022

It's difficult to know where the connection problem could be, mostly because I don't really know how the credentials etc are supposed to be set up for your organization.

However, in order to create a new STM32 project with the latest firmware you could download it from st.com, then in STM32CubeIDE you can go to Help -> Manage Embedded Software Packages -> From Local ... and import the package locally.

Agour.1
Agour.1Author
Associate III
June 30, 2022

Thank You for your reply Markus.

the procedure for credentials entry is tested on 2 more machines and it worked on the first attempt.

My observation is that computers, where STM32cubeide was reinstalled are having this sort of connection problem. Wherever stm32cubeide is installed for the 1st time; no issue is there while connecting and downloading relevant packages.

Right now I created the project on some other computer and brought it back to my machine for continuing my work.

while trying Help -> Manage Embedded Software Packages -> From Local ... i faced the problem mentioned in the attached image. i downloaded the package from https://www.st.com/en/embedded-software/stm32cubeu5.html#get-software

0693W00000Nt7NnQAJ.png 

some how I strongly feel the network connection must work for smooth creation of project. Please provide your support to make network connection work on my machine.. 

Markus GIRDLAND
ST Employee
June 30, 2022

Where did you place the FW package?

I believe the Embedded Software Packages Manager is trying to search for the stm32cube_fw_u5_v110.zip file in C:\Users\USER\STM32Cube\Repository

Aymen CHAKROUN
ST Employee
June 30, 2022

Hi @Markus GIRDLAND​ , @Agour.1​ 

Can you please follow instruction detailed in the CubeMX UM1718:

0693W00000Nt7oFQAR.png 

Regards,

Aymen.

Aymen CHAKROUN
ST Employee
June 30, 2022

And to be more correct, below the step by step procedure to install the patch:

  1. Download the STM32CubeU5 FW from: https://www.st.com/en/embedded-software/stm32cubeu5.html
  2. Put the zipped file en.stm32cubeu5_v1-1-0.zip under your FW repository
  3. Rename the zipped file from 'en.stm32cubeu5_v1-1-0.zip' to 'stm32cube_fw_u5_v110.zip'
  4. Download now the patch from the same address https://www.st.com/en/embedded-software/stm32cubeu5.html
  5. Put the downloaded patch 'en.patch-cubeu5_V1-1-1.zip' in a place other than your FW repository (e.g: your Download folder)
  6. Try now installing the patch 'en.patch-cubeu5_V1-1-1.zip' using the 'From Local…' button

Let me know your feedback,

Aymen.

Agour.1
Agour.1Author
Associate III
June 30, 2022

Thanks a ton Aymen.. it worked..

Can you plz suggest some remedy for my network connection issue..

Peter BENSCH
ST Technical Moderator
June 30, 2022

Sorry for the trouble with the network settings in Eclipse, which sometimes can be a bit exhausting until you finally get it to work.

Is it possible that you work with your machine via VPN?

In this case, with STM32CubeIDE you are "already in your network", so to speak, and should not need any credentials or proxy settings. Instead of Preferences > General > Network Connections = Manual, please try the mode Direct, which ignores the settings for Host, Port etc. and uses your current Windows settings for network access.

After Apply and Close, please check again with Preferences > STM32Cube > Firmware Updater / Check Connection whether the connection is recognised.

Just a reminder - there are three modes in the network settings whose function is sometimes not obvious or misunderstood:

  • Direct: direct internet connection or already setup outside of Eclipse (proxy settings can be set, but are ignored)
  • Manual: internet connection via proxy settings (host, port, etc)
  • Native: internet connection via thge settings of the operating system, i.e. Windows, Linux or MacOSX (proxy settings can be set, but are ignored)

Does it work now?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Aymen CHAKROUN
ST Employee
June 30, 2022

Hi @Agour.1​ ,

Please follow these instructions to collect more details about your network issue:

  • Backup following two folders [e.g rename .eclipse to old.eclipse]:

C:\Users\<use_name>\.eclipse

C:\Users\<use_name>\.stm32cubemx

  • Open STM32CubeIDE 1.10.0 and set as usual your proxy name and password with 'Manual' setup and only for HTTP and HTTPS

  • Click on Apply and then try doing the check connection (try to do twice the check for eventual conflict in the connection test)

  • If the check connection is failed, please attach us the '.ide.log' file founded under: "C:\Users\<use_name>\STM32CubeIDE\workspace_1.10.0\.metadata"

Regards,

Aymen.

Agour.1
Agour.1Author
Associate III
July 1, 2022
Aymen CHAKROUN
Aymen CHAKROUNBest answer
ST Employee
July 1, 2022

Hi @Agour.1​ ,

I'm suspecting a certificate issue with your proxy company.

The other PC Lab (where CubeIDE execution is OK), is also running on Windows 7 ?

Last trial to test:

  • Open the file "C:\ST\STM32CubeIDE_1.10.0\STM32CubeIDE\stm32cubeide.ini"
  • Remove the line -Djavax.net.ssl.trustStoreType=WINDOWS-ROOT
  • Delete your "C:\Users\<usename>\STM32CubeIDE" workspace
  • Delete .eclipse and .stm32cubemx folders
  • Retry to open CubeIDE, setup your usual manual proxy and perform a test connection (may be do the check twice)

Regards,

Aymen.

Agour.1
Agour.1Author
Associate III
July 1, 2022

Hi Aymen

Your last trial worked. Thanks a lot, man. Please see the attached snippet. I am attaching ide log for you to diagnose further.

0693W00000QKFrdQAH.png 

Reply for "The other PC Lab (where CubeIDE execution is OK), is also running on Windows 7 ?" - I have tried two PC with Windows8 and windows7. Please note the fresh installation was done for both of these PCs.

Aymen CHAKROUN
ST Employee
July 1, 2022

Seems your setup is now OK.