Skip to main content
Associate
Jun 6, 2024 9:39 AM UTC
Solved

Unable to upload firmware on Ubuntu 24.04

As described in this post during installation of CubeIDE on Ubuntu 24.04 an error is presented because libncurses5 is not available for Ubuntu 24.04. This can be worked around by using the generic installer. When attempting to upload firmware to an MCU, however, the same error message is given (it is shown as "Could not determine GBD version", but in details the missing libncurses5 is shown). The solution to a similar problem is given in this post, but the solution does not work for the CubeIDE as it requires a specific version of libncurses to be installed.

Any suggestions would be greatly appreciated!

    This topic has been closed for replies.
    Semer CHERNI
    Semer CHERNIBest answer
    ST Employee
    Jun 10, 2024 9:35 AM UTC

    Hello @Lennart 

    First let me thank you for posting.

    I need to mention that the Ubuntu 24.04 is not yet supported by STM32CubeIDE.
    Check the release note of STM32CubeIDE under this link.

    BR,
    Semer.

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    3 replies

    Semer CHERNI
    Semer CHERNIBest answer
    ST Employee
    Jun 10, 2024 9:35 AM UTC

    Hello @Lennart 

    First let me thank you for posting.

    I need to mention that the Ubuntu 24.04 is not yet supported by STM32CubeIDE.
    Check the release note of STM32CubeIDE under this link.

    BR,
    Semer.

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Xynium
    Associate III
    Jan 12, 2025 9:43 AM UTC

    Hello,

    Still have the error, and now "Linux®: Ubuntu® LTS 22.04 and LTS 24.04, and Fedora® 40" are officialy supported.

    BR

    JP

     

    Visitor II
    Aug 20, 2025 1:05 PM UTC

    To fix uploading firmware for the CubeIDE on Ubuntu 24.04 install gdb-multiarch

    sudo apt install gdb-multiarch

    and replace arm-none-eabi-gdb file in <stm32cubeide_1.19.0 install dir>/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.linux64_1.0.0.202410170706/tools/bin/ directory with symlink to /usr/bin/gdb-multiarch. 

    BR
    SP