Skip to main content
MLe M.1
Associate II
Nov 25, 2025 11:00 AM UTC
Solved

Unable to start STM32CubeIDE_2.0.0

Hello,

I can not start STM32CubeIDE_2.0.0.

I have the following error:

D:\ProgramFiles\STMicroelectronics\STM32CubeIDE_2.0.0\STM32CubeIDE;;.
C:\Users\Mich\.swt\lib\win32\x86_64\swt-win32-4966r5.dll: La procedure specifiee est introuvable
Can't load library: C:\Users\Mich\.swt\lib\win32\x86_64\swt-win32.dll
Can't load library: C:\Users\Mich\.swt\lib\win32\x86_64\swt.dll
C:\Users\Mich\.swt\lib\win32\x86_64\swt-win32-4966r5.dll: La procedure specifiee est introuvable

In directory .swt\lib\win32\x86_64 there is only swt-win32-4966r5.dll file.

Why the installer does not put these files?

Do you have any correction please?

Best regards

Michel

ST Technical Moderator
Nov 25, 2025 2:15 PM UTC

Hello @MLe M.1 ,

 

Related to STM32CubeIDE 2.0 Release Note:

Host PC system requirements
Supported operating systems and architectures
• Windows® 10 and 11, 64 bits (x64)
• Linux®: Ubuntu® LTS 22.04 and LTS 24.04, and Fedora® 42
• macOS® 15 (Sequoia), macOS® 26 (Tahoe)
Note: Windows is a trademark of the Microsoft group of companies.
Linux® is a registered trademark of Linus Torvalds.
Ubuntu® is a registered trademark of Canonical Ltd.
Fedora® is a trademark of Red Hat, Inc.
macOS® is a trademark of Apple Inc., registered in the U.S. and other countries and regions.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

5 replies

Andrew Neil
Super User
Nov 25, 2025 11:08 AM UTC

You haven't said what Windows version you're using; also, 32 or 64 bit ?

 

How to write your question to maximize your chances to find a solution

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ST Technical Moderator
Nov 25, 2025 11:15 AM UTC

Hello @MLe M.1 ,

 

Let me thank you for posting.

For more investigation, could you please provide the Operation System used.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
MLe M.1
MLe M.1Author
Associate II
Nov 25, 2025 2:12 PM UTC

Windows 8.1 Professionnel

x64

ST Technical Moderator
Nov 25, 2025 2:15 PM UTC

Hello @MLe M.1 ,

 

Related to STM32CubeIDE 2.0 Release Note:

Host PC system requirements
Supported operating systems and architectures
• Windows® 10 and 11, 64 bits (x64)
• Linux®: Ubuntu® LTS 22.04 and LTS 24.04, and Fedora® 42
• macOS® 15 (Sequoia), macOS® 26 (Tahoe)
Note: Windows is a trademark of the Microsoft group of companies.
Linux® is a registered trademark of Linus Torvalds.
Ubuntu® is a registered trademark of Canonical Ltd.
Fedora® is a trademark of Red Hat, Inc.
macOS® is a trademark of Apple Inc., registered in the U.S. and other countries and regions.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.