Skip to main content
Associate II
Feb 6, 2025 3:24 PM UTC
Question

Unable to Generate Command Line in STM32CubeIDE After Adding AI Network Files

I generated the network code using the STM32Cube.AI CLI and now have network.c/.h files. I want to integrate them into my existing STM32CubeIDE project and use the main() function as mentioned in the documentation("file:///C:/Users/user2/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/9.1.0/Documentation/how_to_run_a_model_locally.html") (attached).

Since the documentation suggests creating a Makefile, I am instead trying to configure it within STM32CubeIDE. Here’s what I’ve done so far:

  1. Added network files: Moved network.c to Src/ and network.h to Inc/.
  2. Included AI Middleware Headers: Added all necessary files from C:\ST\STEdgeAI\2.0\Middlewares\ST\AI\Inc to Inc/.
  3. Linked the AI Library: Configured the linker settings to include the required AI libraries.(https://community.st.com/t5/stm32-mcus/how-to-add-external-libraries-in-stm32cubeide/ta-p/628619)

However, when I try to build the project, I get the following error:

unable to generate command line.

The error seems to be triggered by the following code in the Makefile:

 

 
# Each subdirectory must supply rules for building sources it contributes USB_HOST/Target/%.o USB_HOST/Target/%.su USB_HOST/Target/%.cyclo: ../USB_HOST/Target/%.c USB_HOST/Target/subdir.mk $(error unable to generate command line)

I’m stuck at this point. Is my integration process incorrect? Should I be doing something differently to properly include the AI network files? Any suggestions or workarounds would be highly appreciated!

This topic has been closed for replies.

1 reply

mkothuriAuthor
Associate II
Feb 10, 2025 4:28 AM UTC

?????