UM2217 ADC HAL description not coincide with RM0433 Reference manual in ADC conversion time.
UM2217 ADC HAL description not coincide with RM0433 Reference manual in ADC conversion time.
On page 54 of UM2217 there is the following:
“Sampling time value to be set for the selected channel. Unit: ADC clock cycles Conversion time is the
addition of sampling time and processing time (12.5 ADC clock cycles at ADC resolution 12 bits, 10.5 cycles at 10 bits, 8.5 cycles at 8 bits, 6.5 cycles at 6 bits)�?
On page 926 RM 0433 there is the following:
“The total conversion time is calculated as follows:
TCONV = Sampling time + 7.5 ADC clock cycles
Example:
With Fadc_ker_ck = 24 MHz and a sampling time of 1.5 ADC clock cycles (14-bit mode):
TCONV = (1.5 + 7.5) ADC clock cycles = 9 ADC clock cycles = 0.375 μs (14 bit mode for
fast channels)�?.
From the example in RM 0433 ADC conversion time is one halve of digit capacity.
What conversion time is correct?