Skip to main content
Associate
Jul 2, 2026 9:08 PM UTC
Solved

Two versions of STM32CubeIDE on one PC?

1. 

Is it possible to install two versions of STM32CubeIDE (e.g., 1.9.0 and 1.19.0 or 1.19.0 and 2.2.0) on one PC (Windows)? 
  If so, can I run both versions simultaneously?
    If so, can I program two microcontrollers simultaneously with two programmers?
2.
Is it possible to install STM32CubeIDE and STM32CubeIDE for VS Code on one PC (Windows)? 

  If so, can I run both versions simultaneously?
    If so, can I program two microcontrollers simultaneously with two programmers? 

Andrew Neil
Andrew NeilBest answer
Super User
Jul 2, 2026 9:36 PM UTC

You can install any number of different versions of CubeIDE on one PC, and use them all at once.

You will need a separate workspace for each version.

 

You can even run the same version multiple times - but that requires a separate workspace for each running instance.

 

I don’t know about VSCode.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

3 replies

Andrew Neil
Andrew NeilBest answer
Super User
Jul 2, 2026 9:36 PM UTC

You can install any number of different versions of CubeIDE on one PC, and use them all at once.

You will need a separate workspace for each version.

 

You can even run the same version multiple times - but that requires a separate workspace for each running instance.

 

I don’t know about VSCode.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
beruAuthor
Associate
Jul 2, 2026 10:06 PM UTC

Good news! Thanks a lot.

Andrew Neil
Super User
Jul 8, 2026 12:02 PM UTC
  1.  Is it possible to install STM32CubeIDE and STM32CubeIDE for VS Code on one PC (Windows)? 

See separate thread:

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.