Skip to main content
MMARI.1
Senior II
January 13, 2023
Question

trying to split 16bit number into two 8 bit number uint8_t bytes[2]; uint16_t value = 1234; bytes[0]= value >> 8; bytes[1]= value & 0xFF; what is the wrong in this code . cube ide keep giving compile error .

  • January 13, 2023
  • 6 replies
  • 2650 views

..

This topic has been closed for replies.

6 replies

alister
Senior III
January 13, 2023

The error is likely to be in the context. If you could post the code and the error, it'll save guessing, and most likely, you'll also get some suggestions, e.g. about unions, that'd save code and cycles.

alister
Senior III
January 13, 2023

#include <stdint.h>

MMARI.1
MMARI.1Author
Senior II
January 13, 2023

Great Alister .... thanks ... i already included stdio.h stdlib.h & maths.h its's started working . i think stdint.h inclusion also additional help .

Piranha
Principal III
January 14, 2023
MMARI.1
MMARI.1Author
Senior II
January 14, 2023
uint16_t number11=0;
 
union
{
uint8_t bytes[2];
uint16_t number1;
}memory16bits;
 
union
{
 uint16_t value1;
 
 struct
 {
 uint8_t byt[2];
 
 
 }bytnumber;
 
}pixel;
int main(void ) {
 while (1)
 {
 /* USER CODE END WHILE */
	 pixel.value1 =12345;
 
	 memory16bits.bytes[0]=pixel.bytnumber.byt[0];
	 memory16bits.bytes[1]=pixel.bytnumber.byt[1];
 
 
	 number11 = memory16bits.number1;
 
 
	 HAL_Delay(1000);
	 pixel.value1 =55555;
	 memory16bits.bytes[0]=pixel.bytnumber.byt[0];
	 memory16bits.bytes[1]=pixel.bytnumber.byt[1];
	 number11 = memory16bits.number1;
 
 
 
	 HAL_Delay(1000);
 
 
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}
 
}

Working perfect splitting 16 bit into two 8 bit and recombine two 8 bit into single 16 bit .

how to split four letter " STAT "or " STOP" string into single char and recombine using union and struct ?

Piranha
Principal III
January 14, 2023

There is no string type in C. A string is just an array of char elements terminated with a zero.

https://en.cppreference.com/w/c/language/string_literal