Skip to main content
Associate
March 28, 2024
Solved

🛠️ Troubleshooting STM32CubeIDE Build Issues on Windows Using Command Line 🖥️

Hi,

I've faced an issue while attempting to build the project using the command line in STM32CubeIDE:

./stm32cubeide --launcher.suppressErrors -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data "$WORKSPACE_PATH" -build "$PROJECT_NAME"

Although the build works fine when initiated directly from STM32CubeIDE, I faced the following issue:

***************************************************************************************************************

**** Build of configuration Release for project OSV3_Logic ****
make -j16 all
.
.
.
.
arm-none-eabi-gcc "../Core/Src/Test/unitTest.c" -mcpu=cortex-m4 -std=gnu11 -DUSE_HAL_DRIVER -DSTM32WB55xx -c -I../../Middlewares/Third_Party/coreJSON/core_json.c -I../Core/Inc -I../Core/Inc/Communication -I../Core/Inc/Utils -I../Drivers/STM32WBxx_HAL_Driver/Inc -I../Drivers/STM32WBxx_HAL_Driver/Inc/Legacy -I../Middlewares/Third_Party/FreeRTOS/Source/include -I../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2 -I../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -I../Drivers/CMSIS/Device/ST/STM32WBxx/Include -I../Drivers/CMSIS/Include -I../Drivers/Third_Party/MODBUS-LIB/Inc -I../Drivers/Third_Party/MODBUS-LIB/Config -I../USB_Device/App -I../USB_Device/Target -I../Middlewares/ST/STM32_USB_Device_Library/Core/Inc -I../Middlewares/ST/STM32_USB_Device_Library/Class/CDC/Inc -I../Drivers/Third_Party/W25QXX/Inc -Os -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Core/Src/Test/unitTest.d" -MT"Core/Src/Test/unitTest.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Core/Src/Test/unitTest.o"
In file included from ../Core/Src/Utils/json_handler.c:8:
../Core/Inc/Utils/json_handler.h:13:10: fatal error: core_json.h: No such file or directory
13 | #include "core_json.h"
| ^~~~~~~~~~~~~
compilation terminated.
make: *** [Core/Src/Utils/subdir.mk:28: Core/Src/Utils/json_handler.o] Error 1
make: *** Waiting for unfinished jobs....
In file included from ../Core/Src/Uart/uart_main_mcu_task.c:10:
../Core/Inc/Utils/json_handler.h:13:10: fatal error: core_json.h: No such file or directory
13 | #include "core_json.h"
| ^~~~~~~~~~~~~
compilation terminated.
make: *** [Core/Src/Uart/subdir.mk:19: Core/Src/Uart/uart_main_mcu_task.o] Error 1
"make -j16 all" terminated with exit code 2. Build might be incomplete.

Build Failed. 5 errors, 0 warnings. (took 28s.661ms)

***************************************************************************************************************


Any insights or suggestions on how to resolve this.

Thanks in advance!

#STM32CubeIDE #Windows #Development #Troubleshooting :rocket:

This topic has been closed for replies.
Pavel A.
Pavel A.Best answer
March 28, 2024

To build a specific configuration, use this syntax: project/configuration. 

So  -build "${PROJECT_NAME}/Debug"

 

6 replies

Joe WILLIAMS
ST Employee
March 28, 2024

Hi Mohammadsh

Your case is being handled by the ST Online Support Group now.

Kind Regards

Joe WILLIAMS

STMicro Support

Associate
March 28, 2024

Thanks,

Mohammad Sharabati

Pavel A.
March 28, 2024

> **** Build of configuration Release for project OSV3_Logic ****

When you build from the IDE, is the active configuration Debug by chance?

 

Associate
March 28, 2024

Hi @Pavel A. ,

 

yes.

Could you please guide me on how to run the command in Debug mode via CLI?

 

Thanks,

Kind Regards,

Mohammad Sharabati

Pavel A.
Pavel A.Best answer
March 28, 2024

To build a specific configuration, use this syntax: project/configuration. 

So  -build "${PROJECT_NAME}/Debug"

 

Associate
March 31, 2024

Thanks