Skip to main content
Senior
August 21, 2024
Question

'Transfer Event Generation' settings in 2 places in cubeMX/cubeIDE for STM32U5

Hi,

When using the linked-list DMA, there are two places show the 'Transfer Event Generation', one is in the 'GPDMA1' settings and the others in the 'LINKEDLIST' nodes settings. Are they refer to the same thing? If so, are there any reason to let user set them at two places?

Thanks.

This topic has been closed for replies.

2 replies

ST Employee
August 22, 2024

Hello @diverger, 

Yes, both settings refer to the same thing.

However, GPDMA settings apply on the totality of the DMA controller and the linked list settings are more fine-tuned.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
divergerAuthor
Senior
August 22, 2024

Hi,

If they refer to the same thing, then there are possibilities that they are set to different values. In that case, which one will take effect?  That is, how they affect the final code, what's the logic behinds?

Thanks.