Skip to main content
Associate
August 6, 2024
Question

Touchgfx issue with uart not working good

Hi,

I am a beginner to touchgfx, i am using stm32u599vjt6.

I am having an issue using uart with touchgfx.

My function is to check different conditions every time my handle tick function is called and after checking i need to send some commands from uart.(if one condition satisfies one command another satisfies then another)

Uart is ok when i am sending one string for one handletick fun call but the data is being manipulated when i am trying use uart 2 times(sending 2 strings) in the same handletick func call. 

I hope you understand my issue.

please suggest me a way to solve this issue.

 

 

    This topic has been closed for replies.

    2 replies

    Associate
    August 6, 2024

    FYI: I am using 9bit uart in interrupt mode 

    Karl Yamashita
    Principal
    August 8, 2024

    You forgot to attach your code

    If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source