Skip to main content
sanju
Associate III
December 6, 2022
Question

Total ROM and RAM usage

Hi all,

i have tried same project in two different IDEs( Keil and STM32CUBEIDE). i am confuse that why they both are telling different usgae for RAM and ROM.

Keil map file says:

Total RO Size (Code + RO Data)        21156 ( 20.66kB)

 Total RW Size (RW Data + ZI Data)       2360 (  2.30kB)

  Total ROM Size (Code + RO Data + RW Data)   21284 ( 20.79kB)

STM32 Cube IDE says:

0693W00000WKI1AQAX.pngwhy the difference is there between these IDEs. application code is same and HAL code is generated by STMCUBEMX for both IDEs.

Post edited to adhere community guidelines.

This topic has been closed for replies.

1 reply

S.Ma
Principal
December 6, 2022

Programming101:

Not all compiler and linker are equally performant in memory footprint.

Compiler options will also affect footprint results. It is called benchmarking the compiler toolchains.