Skip to main content
FPare.1
Associate
May 19, 2025 7:46 AM UTC
Solved

Toolchain Manager is painfully slow

The Toolchain Manager takes 5–10 minutes to load the toolchain list, even with only a few installed.
It happens every first time I open it after launching the IDE.
If I close it and reopen it during the same session, it loads instantly.
But if I restart the IDE, the delay returns.

Is this normal behavior?
If so, is there anything that can be done to speed it up?

STM32CubeIDE
Version: 1.18.1
Build: 24813_20250409_2138 (UTC)

This topic has been closed for replies.
Souhaib MAZHOUDBest answer
ST Technical Moderator
May 19, 2025 2:14 PM UTC

Hello @FPare.1 

Actually, this is a normal behavior that toolchain manager takes some time to load toolchain lists.
Fetching time really depends on the amount of repositories defined on the 'Available Software Sites' page.
It's important to note that Eclipse fetches repository files in the background during startup, so I recommend waiting for a moment after the startup.

KR,

Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Souhaib MAZHOUDBest answer
ST Technical Moderator
May 19, 2025 2:14 PM UTC

Hello @FPare.1 

Actually, this is a normal behavior that toolchain manager takes some time to load toolchain lists.
Fetching time really depends on the amount of repositories defined on the 'Available Software Sites' page.
It's important to note that Eclipse fetches repository files in the background during startup, so I recommend waiting for a moment after the startup.

KR,

Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.