Timer interrupt is enabled but it is not entering the interrupt handler
I'm working on STM32G030 in STM32CubeIDE without using the HAL( using Low layer). In that i have enable a timer interrupt using .ioc file (hardware file). When i put a break point in the interrupt handler which is in the stm32g0xx_it.h file, it is not entering the handler.I have also tried by giving the priorities to the interrupt but still it won't work Here is the snippet of the code:
GPIO_InitStruct.Pin = IC_mode_Pin;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
GPIO_InitStruct.Alternate = LL_GPIO_AF_2;
LL_GPIO_Init(IC_mode_GPIO_Port, &GPIO_InitStruct);
/* TIM1 interrupt Init */
NVIC_SetPriority(TIM1_BRK_UP_TRG_COM_IRQn, 0);
NVIC_EnableIRQ(TIM1_BRK_UP_TRG_COM_IRQn);
NVIC_SetPriority(TIM1_CC_IRQn, 0);
NVIC_EnableIRQ(TIM1_CC_IRQn);here i have taken TIM1 interrupt. And here is the my Interrupt handler.
void TIM1_CC_IRQHandler(void)
{
/* USER CODE BEGIN TIM1_CC_IRQn 1 */
if(TIM1->SR |= TIM_SR_CC3IF) // When a capture occurs, the corresponding CC1IF flag is set
{
TIM1->SR &= ~TIM_SR_CC3IF; //clear the flag by writing it to 0
TIM1->CCMR1 |=TIM_CCMR1_OC1M_2; //Force inactive level
TIM3->CR1 |= TIM_CR1_CEN; // Starts the counter
}
/* USER CODE END TIM1_CC_IRQn 1 */
}Can someone explain why does it not enter the handler that is assigned to it.