TIM16 never calls interrupt handler in STM32WLE4
Hi
I've configured automatically from IOC timer TIM16 as it is more basic timer and I need basic funcionality: do some action on timer interrupt, I use HAL driver, but handler is never called.
initialisation is simple:
void MX_TIM16_Init(void)
{
/* USER CODE BEGIN TIM16_Init 0 */
/* USER CODE END TIM16_Init 0 */
/* USER CODE BEGIN TIM16_Init 1 */
/* USER CODE END TIM16_Init 1 */
htim16.Instance = TIM16;
htim16.Init.Prescaler = 511;
htim16.Init.CounterMode = TIM_COUNTERMODE_UP;
htim16.Init.Period = 50000;
htim16.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim16.Init.RepetitionCounter = 0;
htim16.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
if (HAL_TIM_Base_Init(&htim16) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM16_Init 2 */
/* USER CODE END TIM16_Init 2 */
}
Timer is running , I can see it's changing value when read. It's set to reload periodicaly, it does that, interrupt is enabled, given higher priority than others, just in case. Vector table is properly initialised. But interrupt handler never is called. What to check, any ideas?