Skip to main content
Associate II
Apr 25, 2025 8:21 AM UTC
Question

"There is no active editor that provides an outline"

Hello everyone, I am on Windows 11 and am using STM32CubeIDE version 1.18.0 (also tried on verison 1.18.1). I have logged into myST within the software as well (through Help->STM32Cube Updates -> Connection to myST). I can edit the pins in the .ioc file just fine, but I cannot open the code editor; I keep getting this particular error. I have tried closing and reopening the app, restarting my computer, deleting and reinstalling and downgraded the version to try to verify if the problem was in the software. 

Can someone help me? 

Screenshot of the app: 

deta_0-1745569245869.png

 

 

This topic has been closed for replies.

7 replies

Andrew Neil
Super User
Apr 25, 2025 8:27 AM UTC

@deta wrote:

I can edit the pins in the .ioc file just fine, but I cannot open the code editor


What, exactly, do you do when trying to open the code editor?

It looks like you haven't yet generated any code to edit - so have you tried generating code first?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
detaAuthor
Associate II
Apr 25, 2025 8:29 AM UTC

Yes, I click Ctrl+S to save my pin configurations and get the prompt that the system will generate the code, and if I'd like to change to C/C++ perspective. Which is what should happen. But then this error occurs.

Andrew Neil
Super User
Apr 25, 2025 8:37 AM UTC

So no code is generated?

What happens if you click the button for the C/C++ perspective?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate
Jul 26, 2025 9:17 PM UTC

I was also facing this issue. No code is being generated. 

Consider updating the IDE. My issue was fixed after I updated it. During the update, some necessary toolchains was downloaded.

Andrew Neil
Super User
Jul 27, 2025 9:09 AM UTC

Note that you're replying to a post from four months ago.

 


@rahgirrafi wrote:

No code is being generated. 


So was that the issue described in this pinned post:  [Resolved] STM32CubeIDE project creation issue ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.