Skip to main content
MSale.1
Senior
June 22, 2022
Question

There are many issues and bugs with the STM32 Cube FW_H7_V1.10.0.

  • June 22, 2022
  • 2 replies
  • 1373 views

If i try to use this BSP of the above version and integrate with project generated from Cube IDE then many issues happen. for example problems with STM32H747_Discovery_Camera.

Also integrating the touch controller with touchgfx is not working and instead of providing ideas here maybe you try it by your self on some discovery boards and show us or simply back to the older BSP Version.

This topic has been closed for replies.

2 replies

MM..1
Super User
June 25, 2022

You mix two not relevant thinks. FW_H7 and BSP. Try show code part and what dont work instead for example ...

Tesla DeLorean
Guru
June 25, 2022

The underlying problem here is that the code is often not well tested, and the H747I-DISCO doesn't have the camera mounted, so it's a random variable, so support is unlikely to be broad.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..